Dear,
i use the BQ51025-EVM to output 5V 2A with BQ500215-EVM.I had changed some components on BQ51025-EVM.
If i put the RX-EVM on center of TX-coil,it can not work well.
i need to shift a little location,and it can work well.
if i change the resonance capacitance of BQ500215 from 0.247uF to 0.315uF,It had work well on any location.
but I use BQ51013B-EVM on BQ500215-EVM,It only work well on center of BQ500215-EVM.
could you help to fix this issue of 5V 2A application?
thanks.