Hello everybody.
Somebody could tell me the main difference between these two receivers (appart from one has adjustable output)? Any help will be usefull.
Thanks in advance!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.) The bq51020 is a larger device with better thermal performance, lower thermal rise at 5W output. Larger package and higher number of solder balls.
2.) The bq51020 is an adjustable output device from 4.5V to 8V. The bq51013B is fixed at 5V out.
3.) Bq51013B has a QFN package option, preferred by some customers.
4.) Bq51021 will support I2C communications with a host controller, (020 does not have I2C).