Hello,
I am trying to measure the power being dissipated in the Tx coil. I have connected an oscilloscope between TP1 and TP2 to measure the peak to peak voltage across the Tx coil and then use the resistance of the coil to find the power. However, I notice that when I attach a the oscilloscope to working system, the input current into the system increases, which means that system efficiency decreases. Is the oscilloscope placing an extra impedance on the PA/Tx coil and will it effect my power measurement? Can the TP I_Sense be used to measure the coil power?
Thanks,
Jason