Hey All,
I'm designing a Qi compliant inductive charger Rx circuit using the BQ51003 for a wearable. Here are the questions I have:
1) Can the FOD pin be used as an internal signal to monitor the output current?
2) What is the ratio between RFOD and R1 supposed to be to ensure the proper FOD voltage is measured? My output current is 50mA
3) Can the 3 state driving circuit also be used with the temperature limiting circuit on the TS-CTRL pin?
4) I need to regulate the output from 5V to 4.2V to meet the maximum battery charging voltage specifications. How would an LDO or zener diode effect the current limiting/battery charging capabilities of the device?
Thanks!