I used bq500212AEVM-550 evaluation board with bq51050EVM-764 and now is working fine.
But I can not getting to work with bq51003EVM-764!!! They are compaible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I used bq500212AEVM-550 evaluation board with bq51050EVM-764 and now is working fine.
But I can not getting to work with bq51003EVM-764!!! They are compaible?
Thank you, Upal.
My setting:
JP2: LOW
JP1: LOW
JP4: VZ
JP3: EN
TS-GND(R3); 10 kohms
ADJ-GND: 600 ohms
Without battery,
bq500212AEVM
D5(LED) : It is Flashing
D7, D9: off
bq51003EVM
D1: on with small flashing
With battery,
same withou battery, but the receiver side, the D1 is turned on without small flashing.
See the scope.