hopefully this isn't too simplistic a question but I'm not getting something that seems fundamental....
using the EVMs noted out of the box and without modification, I'm trying to set up a measurement. instead of electronic load we are using power resistors of 3 to 100 Ohms (numbers based on I-V of 2000 mA-hr Li+ battery charge profile; power should peak at 5W around 3.5 Ohms for battery charging). for the nominal 5V/1A output we are seeing currents from receiver that change with load, but they are de-rated for reasons I am not getting. For example the 5 Ohm load should give us 1 A but we're getting 0.6A or so. We checked ILIM and FOD and potentiometer (and varied this pot, could make current go smaller).
for 51020 data sheets show 1A outputs for what appear to be 5 ohm loads (electronic), but these all seem to use a different transmitter that can run off 19V power. is the problem simply that the '212 transmitter is undersized? datasheet says it will draw 1.5-2 A which I assume would compensate for efficiency penalties.
any help appreciated for what seems like a problem maybe I'm looking at wrong or thinking too much. or this a matter of fine tuning, that out of the box they do not deliver rated performance until you tweak them?
thx, cm
PS- On a side note what does the bq51x2x EVM GUI do for someone?