I’m currently evaluating TI wireless charging technologies.
I’m specifically looking at if the 10W solution with bq500215 and bq51025 could be used for our devices.
The basic requirements are:
Input: 13.5V±0.5V
Output: 13.5V±0.5V
From the datasheets of bq500215 and bq51025, it seems it is limited to 12V input and 10V output.
Would you be able to help answer the following questions:
-
Can bq500215 EVM be modified to accept 13.5V±0.5V input?
-
Can bq51025 EVM be modified to give output at 13.5V nominal? Such as modify R6, R7?
-
What is the recommend inductance for the receiver coil to give 13.5V output?
I’m hoping that by using the TI EVMs, we could get a working prototype for our current device. Could you help?