Hi all,
I made this circuit but can't receive power. Can you tell me are the values of C19 and C21 correct and if not what should be?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I made this circuit but can't receive power. Can you tell me are the values of C19 and C21 correct and if not what should be?
Also, the FOD circuit doesn't look correct. You will need to have a Ros resistor connected between RECT and FOD pins. Also you need a resistor from ILIM to FOD. Please refer to bq51013B datasheet for recommended application circuit. If you are not going to use the FOD function, you can use the same value as in below EVM.
http://www.ti.com/lit/ug/sluua44a/sluua44a.pdf
If you want to tune FOD with your system, the below tool can help you with it. There is a detailed manual inside the tool.
http://www.ti.com/lit/zip/sluc577
Plus, the 7.5k ILIM resistor will only give you ~30mA ILIM.
Thanks,
Wenjia
Hi Wenjia,
Thanks for answers. I calculated 238nF and 3.4nF and put that. Should that work even if I didn't correct FOD circuit for now?
Best regards,
Darko
Darko,
Even if you don't use FOD, you still need to have the resistors connected to the right pins. You can start with the value on our EVM.
Thanks,
Wenjia
I made changes, capacitors 200nF and 2nF and resistors connected to appropriate pins but nothing. Do you think coil is ok? What kind of signal I should have on coil.
Darko