Hi,
we are using BQ51050BRHL to charge a small battery that requires only 35 mA fast charge current.
Adjusting the various component the BQ51050BRHL works fine.
For most of the time, the system powered by the battery drows only 4 uA, consequentely any additional current should possibly be avoided.
However, when the receiver coil is not on the transmitter coil (no wireless power present), we found that the BQ51050BRHL drows around 170 uA.
Is this wright? or this current should be maximum 20 uA as indicated in the data sheets 8.5 Iq?
What should be the state of the various control pin in order to minimize this current?
Thank you