I've sent this question to the support, and their advice was to ask here...
We have built a prototype Qi receiver using BQ51050B. At some battery levels (in the middle), the receiver turns OFF every 3-30 seconds, and ON after about 2 seconds.
We have monitored the outgoing communication and it ends with packet 02 04 06, meaning "End Power Transfer" with reason "Over Voltage" (and correct checksum). The documentation for BQ51050B says that this packet is never sent (bq51050b-557127.pdf page 23 Table 1).
Can someone please explain what we need to check or fix in order to avoid "Over Voltage" error?
When we look at the RX coil's voltage, sometimes it goes above 11 Volts just before turning off, other times it seems to stay well below 8 Volts. Also the frequency is around 150kHz most of the time, but rises up to ~200kHz just before disconnect.
The Rfod and Ros resistors have no effect on this behavior (tested Rfod from 100 to 400 Ohm, Ros from 10k to 100k). The coil capacitors have no effect.
It seems that the less inductive the coil is, the better (we have coils 20, 14 and 10 uH). Also partially inserting a ferrite from another coil between the TX and RX coils seems to help a bit, but not always.
Other than the turning OFF and ON, the charging proceeds as designed. We have set Ilim to 400mA, and Iterm to 75 mA.