Good morning, I need to try my BQ500210AEVM-550 with a the coil: TDK WR221230-36M8-G, much smaller and with different L, R, Power than WR760308111 actually mounted on the board.
My question are:
- I need to limit power to 2,5W, is it feasible to use PEAK-DET (pin 1) and the circuit employed in TIDA-00415 to limit voltage pin to 1,75V, or there is other methods to do that?
- to tune the resonant (100KhZ) circuit to the new inductance, I have to change C27, C28, C29, C30 to new values, correct?