Hi, I am trying to implement a wireless charging solution with a predetermined rechargeable battery that needs to be charged at 3.1 V. Will this chip regulate its output to 3.1 V or does it always supply a constant 4.35 V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I am trying to implement a wireless charging solution with a predetermined rechargeable battery that needs to be charged at 3.1 V. Will this chip regulate its output to 3.1 V or does it always supply a constant 4.35 V?
Lucas,
The bq51050B has a charge termination at 4.2V. What that means is it will go to whatever the battery voltage is and begin to charge. As the battery approaches 4.2V, it will go into taper mode (current is reducing) until it reaches the termination current. Based on this, the termination would not occur as normal taper, and the control would have to be external. There is a 10 hour maximum charge time as well.
The bq5105XB wireless chargers have a precharge threshold of 2.9-3V. That means, when the battery is below that threshold, it will be charging at a lower current.
Is your battery specifically rated as a charge at 3.1V or is that the "nominal" voltage. Review the battery specification to verify.
Running a battery at full charge current at or above it's specified maximum voltage is not recommended. Please review the battery specification very carefully.
Regards,
Dick