Other Parts Discussed in Thread: BQ500212AHi, Dick
I am experimenting with Rx 10mm and Tx 15mm coil (not Qi-compliant) using the TIDA-00334 reference design. Tx coil has a large temperature increase (at f~110kHz) because of the small coil, so I am trying to set the current limit of 0.4A using the I_SENSE of Tx side. In order to use the current limit, it looks like there is a need to activate the PMOD. When I set a PMOD resistor of Tx and pull up the FOD of Rx to RECT, it looks like I_SENSE of Tx has a threshold of 2V. By changing the current detection resistor from 20m-ohm to 100m-ohm, it appears to be the current limit is set at 0.4A. I would appreciate it very much if you let me know the information around this. Thank you.
Regards,
Akio