Dear all,
I am currently designing a wireless charger.
First, I thought I would use a BQ51013B for the wireless power with a BQ24250 for charging the battery.
Now, I have just seen the BQ51051B which can combine both features (wireless power + charger).
My question is : with the BQ51051B, could I connect the load while charging ? With the 2 IC solution, I am sure I can do both at the same time but it is not really clear with the 1 IC solution.
Except that the BQ24250 has I2C connection, what are the differences between the 2 designs?
I use a 1 cell LiPo battery (3.7V, 1150mAh) and the system load is up to 150mA but the current can strongly vary over time.
Best regards,
Christian