Hi,
I try output of bq51025 change 7V to 10V.(for 2s charger system.)
So,I can change 10V.
When I set the load to 0.45A ,waveform is unstable(Attachment picture).
Why is this such a waveform has appeared ?
Is this something that can be improved ?
(at bq51025EVM schematic,add a capacitor,this volume is 0.1uF)