Hi, I am considering to buy bq501210 EVM.
I might be the first one asking about bq501210 since it came out lately.
According to the datasheet, bq501210 chip is compliant with WPC v1.2
And as far as I know, WPC v1.2 enables resonant mode.
1) If it is, Is bq501210 EVM possible to enter resonant mode? (What frequency?) transfer power to the receiver at 28mm separation from the transmitter?
2) Then, is bq501210 EVM possible to transfer power to the receiver at 28mm separation from the transmitter?
3) What kind of modification is required to the receiver side to enable resonant transfer?