Hello,
I would like to implement the temperature sense function of the BQ51003 and set a temperature range of 0 to 50DegC. I'll set the resistors and NTC on the TS-CTRL line to do so.
My question is, if I have the device on the charger, it should shut down when the temp reaches 50DegC. But if the device remains on the charger, will it begin to charge again when the temp drops below 50DegC or do I need to remove and replace the device to get it to begin charging again?
Thanks
Craig