Hi!
Wireless charging has giving me troubles lately. For my device I need to find solution for wireless charging of small LiIon battery. Supply/charging voltage is 5V and charging current is max 500mA.
Problem is in Rx coil. It has to be small to fit the device. Square coils can be up to 15x20mm, and round coils up to 10mm OD. Charging distance must be 5mm or more (there is 2mm wall thickness for charger, and another 2-3mm wall thickness of the device itself). Tx coil can be of any size as the dimensions of the charging station is not critical.
I have contacted various Asian companies that sell various Rx/Tx coils, but none seems to have an answer to my problem. I'm guessing because they are mostly re-sellers.
If anyone can appoint me in the right direction how to begin to solve this problem, I would greatly appreciate.
Creating my own pcb is also one of the possibility, but I would prefer standard solution.
Thank you in advance!
Best regards,
Sasa