Dear all,
I am testing my wireless charger with BQ500212A and BQ51051B. The battery can be charged but its charge current is not what I expect.
If I understand correctly, the charge current is set by the sum of resistors R1 and Rfod (that are called Rlim). Then, Icharge = 314 A*ohm / Rlim. The Rfod is 200 ohm and I tried to have R1 = 470 ohm and 330 ohm that gives for Rlim 670 and 530 ohm. So I expected the following current :
- with 670 ohm : 314/670 = 469 mA and I got only about 220mA
- with 530 ohm : 314/530 = 592 mA and I got only about 265mA
I saw that JEITA specicification gives only half the current if the temperature is too cold or hot which could have been the answer to my question... but I measured the TS/CTRL pin and I got about 800mV during the 24 ms of TS measurement which is 0.8/2.2 = 36% of Vtsb. This value is between 19.6% and 47.8% and if I understand correctly, it means the temperature is normal...
Since I do not find any information about the Ros resistor (between RECT and FOD), I put 1 kOhm.
What value should I put for this resistor?
Anyone has an idea about my current charge issue?
Thank you in advance,
Best,
Christian