I am using the bq51025 wireless Receiver chip, the design based on the evm circuit diagram. I cannot get it to start up with a load connected. It starts o.k without a load and then after start up I can connect the load but i can only draw about 300mA max which is much less than it should deliver