Other Parts Discussed in Thread: BQ51025EVM-649, BQ51025
D2 green LED does not flashes but staying ON as the input power (12V) is connected.
Charging does not start. No response at all when I put any Rx on the coil. I can hear strange sound is generated from the board, maybe from the beep speaker.
(I use a BQ51025EVM-649 and a smartphone equipped with WPC v1.1 antenna module)
I found this malfunction this morning. Only yesterday there were no problems in power transfer.
In user's guide document, it is stated that D2 is ON during power transfer and during "fault conditions".
As the EVM does not transfer power to Rx, I assume that something is wrong but I cannot find what kind of fault happened to my EVM.
Does anybody have the same or similar problem with me?
Please give me advice about possible causes on this trouble.
Thank you.