This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51020: BQ51020 OVP Condition

Part Number: BQ51020

Hi

I want to know about OVP condition of bq51020.

below comment is in datasheet of bq51221. Is it apply to bq51020 equally?

- bq51221

Over Voltage : 0x04 : VRECT target does not converge(3)


(3) If the voltage on the RECT pin does not reach the required value (typically 8 V) within 64 error packets
during startup (weak coil coupling), the receiver sends EPT-OV and the transmitter will shut off.