Other Parts Discussed in Thread: BQ500212AEVM-550, TIDA-00669, TPS63050
I have a design based on TIDA-00329 using the BQ51050B. I have a boost converter (MCP1624) and an LDO coming off the Battery line in addition to the BQ1050B. I have attached a picture of the schematic for the LDO and boost converter.
I am unable to get the battery to charge while the boost converter is attached if the battery voltage is very low and engages the Li-poly's low voltage cutoff protection circuit. It does not matter what voltage is on the enable pin of the boost converter. If I take off the boost converter, I can charge the battery even when the low voltage cut-off has engaged. If the battery low voltage cut-off does not engage, I can charge the battery with the boost converter attached. I can charge the battery from any state when it is directly connected to the TIDA-00329 design or BQ41040BEVM-764 I have normal operation if the battery has been charged elsewhere and attached to this circuit.
I am using a BQ500212AEVM-550 as a transmitter. In all the above cases, the green LED on the transmitter blinks indicating power transfer. In the case of the boost converter is attached and the battery's low voltage cut-off is engaged, the transmitter still thinks it is transmitting but the voltage on the battery only goes up to 0.5V to 0.6V and very small current (about 5 uA) is found going between the BQ51050B and the battery.
I have tried using the BQ41040BEVM-764 to adjust current limiting and termination settings but have had the same results. I am baffled by this as there is a boost converter attached similarly in TIDA-00669 500mA wireless charger Booster Pack with Gauge Reference Design. Do I need the Gauge to better isolate the battery for this to work? It seems like the charger isn’t really trying to get to the charge voltage.