Other Parts Discussed in Thread: BQ51010B, TIDA-00318
Hello,,
I have received this reply from a TDK applications engineer:
"You cannot use the WR202010-18M8-ID with this design as it is written. The bq51010b is for use with a Qi compliant Tx coil which this 20 mm round Rx coil will have a lot of difficulties using due to the physical size mismatch. I know TI has other chipsets which are geared for lower power applications and use a smaller Tx coil. Additionally, this coils is modified to be optimized with an IDT chipset so the inductances are not quite what the TI chipset may require. But you can discuss with TI."
(1) Will this coil work with this chipset? We require this small coil. If not, is there another solution?
(2) Does this coil which is "optimized for IDT chipset" have suitable inductance for this TI chipset?
Thanks,
Billy