Other Parts Discussed in Thread: TPS63051, BQ51010B,
Dear All,
I am trying to make a custom wireless power receiver (altium project attached) using BQ51010B and TPS63051 buck boost regulator to get 3.3V output.
I have thoroughly reviewed the documentation of both the ICs and selected the components as recommended. To get charge current (I_BULK) of 0.5A; I have selected R_ILIM. I am using 7.5uH (732-6211-ND) coil from Wurth.
Seemingly there is not much complication in the circuit but when I tested my Rx circuit with the BQ50002EVM-607; I get no voltage on BAT (pin4) of BQ51010B and neither obviously I am not getting anything at the output of TPS63051 as well.
Also I have some specific questions as well:
1. I have noticed a mistake in the design that I am trying to put the Rx Coil directly on the AC1 and AC2 terminals of the chips and the resonant caps are being bypassed. So my question is; what is the role of these resonant caps; are they really important that if we bypass them; we won't receive any power? Any literature on this?
2. I have not put any rechargeable battery or the load, I think the output voltage should have still be appeared. Right?
Can anyone please have a lot at my schematic and suggest me where the problem might be.
Thanks for your time.