Other Parts Discussed in Thread: TPS63051, , BQ50002A, BQ500511A
Dear All,
I am working on this building a simple and compact wireless receiver using BQ51050Band trying to get the regulated 3.3V using TPS63051. I have also built a PCB but I am not getting any output on BAT (pin4) of BQ51050Q and neither on Vout (pin4) of TPS63051.
Here is the schematic of BQ51050B
Charging current has been set to 500mA and 10% termination current.
BAT voltage is being regulated using TPS63051 as shown in schematic below:
I am using 732-6211-ND coil (7.5uH) from digikey as a receiver coil.
On the transmitter side, I am using standard BQ50002EVM-607 from TI and I did not do any changes on Tx side; just supplied it with 5.0V supply and testing with the receiver (schematic shown above).Please note that I have not connected any battery on BAT terminal? Does it make any difference? Also if the L' is not properly calculated; the values of C1 and C2 might be wrong; so how big a difference should it make on the performance.
Any suggestions how to proceed with the debugging?
I will be really obliged if someone takes his time to review and let me know why the Rx circuit is not working.
Thanks