Other Parts Discussed in Thread: BQ500511A, TPS63051
Hello everyone,
I had posted it earlier as well but could not get satisfactory explanation about my error.
I am testing my custom made BQ51050B based receiver which is being powered up using BQ50002EVM-607 Tx. Here is my initial schematic:
I am using 732-6211-ND (7.5uH) Rx coil (although the caps in the schematic are for 8uH coil:: Does that make much of a difference?)
The problem is that; when I start the BQ50002EVM-607 Tx (with Rx coil placed on top); I hear buzzer sound and Green LED blinks (at about 1.25Hz) indicating that the power is being transferred. Charging LED on Rx board also lights up. This happens for few seconds after which the Green LED(D6) stops and D5(RED LED) lights up and the charging LED on Rx also stops. It means some error occurred (I am unable to figure out what is the error).
Here are the scope captures(Vrect in Yellow and V_TS in GREEN) I got:
D5 (RED) LED lights up at the time when the voltages drops. If we see the datasheet it seems like a TS_GND fault.
Bill (Application engineer at TI) had suggested to increase the R_FOD from 140 ohm and shorting R23 on Tx EVM to disable FOD functionality.
I shorted R23 on Tx EVM and increased R_FOD from 140 till 1000 ohm on custom Rx board but the problem remains the same.
I have tested with drained and semi-drained 3.7V Li-Ion batteries. Same error
I tried with applying 40mA load across the battery terminals-Same error
After few attempts; now even the charging LED on custom Rx board has stopped to lit up which used to light up for at least few seconds before.
Please help me in this regard. I really need to get it working asap.
Thanks