Other Parts Discussed in Thread: BQ500511, BQ50002, , BQ50002A
Vrect reaches the correct voltage at power up and is stable under no load, however when I connect a load of approximately 200mA Vrect starts to oscillate, period is aprox 2seconds. I am using my own coils for transmitter and receiver based on the wurth 760308111 (transmitter) & wurth 760308103204 (receiver) both as used in the Texas EVM. However with the wurth coils the effect is much worse and the transmitter switches off aprox every 2 seconds and then back on again.
If I disable the CM_ILIM feature by pulling CM_ILIM high and power from an IDT evaluation kit transmitter, Vrect stays stable and the receiver works well. When powered from the Texas transmitter (bq500511 & bq50002) my receiver switches off. It probably expects communications from the receiver; it doesn’t seem from the datasheet that this function can be switched off in the transmitter.
How can I make Vrect stable?