Other Parts Discussed in Thread: BQ25100, BQ51003, BQ51013
I have a BQ25100 behind a BQ51013B (schematic similar to some ref design given by TI).
The current charge on the BQ25100 is set to 200mA.
If i put externaly 5V on the BQ25100 input, the charge current is ok : 200mA.
When i try to charge from the wirless power side, i have only 60mA.
What can be the limitor factor on the BQ51013B ? The Rilim is ok (1k2 + 196 should be around 225mA).