Hi!
I'm designing a wireless charging unit for a pace maker.
I have designed it with the Rx coil -Vishay(IWAS-4832FF-50 48mm × 32 mm) one of the coils mentioned in the data sheet. But now I need to compact the circuitry so I thought of moving into a smaller Rx coil.
I'm uncertain how I should select the inductance(Ls) , DCR,Q parameters of the coil in addition to the coils mentioned in the data sheet itself.
Ex: If I used this TDK Rx part WR221230-36M8-G
dimensions - 22mm×12mm | thickness 0.87 mm
Inductance - 27.9uH (at 1Vrms/100kHz)
DCR - 1.21
Thankyou!