Other Parts Discussed in Thread: BQ51025
Hello,
we got an issue with our own design of the bq501210 wireless charger. Our design ist pretty much similar to the EVM board.
Our Problem is, when we pair it with an IDT 15W receiver it only transfers 2-4W and the receiver only make 5V output.
With the EVM board everything went perfect and we got 12V out at the receiver.
Maybe the mode switches from 15W to 5W?
We excluded some parts of the evm circuit. For example the USB stuff with the D- and D+ resistors. But we tested this change at the EVM Board, it still worked.
Does this make a difference?
Moreover we canged little things like values of capacitors, but only exchanged them, for example, a 47µ with 5 10µ. Should be fine?
Which parts of the circuit are essential for this different transfer modes? Are there certain values who are responsible for the different transfer modes?
Thank you in advance!