This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMS320C6678: input clock requirement in internal DDR3 PLL sysbsystem

Guru 14710 points

Replies: 3

Views: 751

Part Number: TMS320C6678

Hi,

Just a quick confirmation about input clock requirement in internal DDR3 PLL sysbsystem.
Here is a snippet from C6678 datasheet. The requirement for DDR3 clock pins is 40Mhz(min), but because of PLLD, the clock can be smaller than 40Mhz just before PLLM input stage. I could not see any related restrictions in datasheet, so believe it should be ok, but please let me confirm just in case. Also, I would like to know the clock speed requirements/usage note about the inside of other PLL sysbsystems (Like main PLL, PA PLL, and etc..)  if you have.

Best Regards,
Naoki

  • Hi Naoki,

    I've forwarded this to the design experts. Their feedback should be posted here.

    BR
    Tsvetolin Shulev
  • Hi Naoki,

    The 40MHz lower limit is not associated with the PLL. That is the lower limit of the LJCB clock input buffer associated with the DDRCLKP/N pins. You cannot use a lower frequency then the 40MHz specified for the DDRCLKP/N input with the C6678. 

    Regards,

    Bill

    If you need more help, please reply back. If your question is answered, please click  Verify Answer 

  • In reply to Bill Taboada:

    Ok, Good to know that. Thank you for your clarifications.

    Best Regards,
    Naoki

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.