This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

RTOS/TDA3XEVM: Own Driver for TLV320AIC3109 audio codec

Expert 1055 points

Replies: 14

Views: 1236

Part Number: TDA3XEVM

Tool/software: TI-RTOS

Hi Everyone ,

I am working on a custom board using TDA3XX as reference board , which has audio codec TLV320AIC3109 . I knew that TDA3xx doesnt have support for McASP driver.

I like to know is there any way where we can write own driver / code for TDA3XX audio support  for the given audio codec .  I also like to know whether is there any code we can refer and start writing the driver

Thanks & Regards ,

V.B.Surendar

  • Hi Surendar,

    please check if this thread can help you:
    e2e.ti.com/.../2366089

    Regards,
    Yordan
  • In reply to Yordan Kamenov:

    Hi Yordan,


    Thanks for sharing the thread .

    I have already gone through that thread . My doubt is, there is a sample program for audio in starterware for TDA2X . I like to know whether it is possible to port that code in custom TDA3xx board [which has audio codec] for checking .
  • In reply to Surendar V B:

    Hi, ,

    Starterware expert is notified and will comment directly here.

    Regards,
    Mariya

     Be sure to read the Forum Guidelines and FAQ.

  • In reply to Mariya Petkova:

    Hi Surendar,

    We have the example in starterware which has support for aic3106 codec which is present on tda2xx board.
    Its the codec of same series you are using, but you might have to check the differences between them while porting.

    Regards,
    Prasad
  • In reply to Prasad Konnur:

    Hi Prasad,

    We are using aic3109 codec , I like to know what kind of changes I need to do in the starterware example to port to TDA3XX

  • In reply to Surendar V B:

    Hi Surendar,

    Please refer the post below.
    e2e.ti.com/.../2378559

    I have mentioned the steps required to port example to Tda3xx.

    Regards,
    Prasad
  • In reply to Prasad Konnur:

    Hi Prasad ,

    I have updated as per you mentioned in the post , in the same reference program and I have compiled for tda3xx .

    But the appimage get stuck before "McASPTxClkStart" function , and I also not getting any input  master clock for the audio.

    Can you kindly help me on this

  • In reply to Surendar V B:

    Hi Prasad ,

    is there any update on this
  • In reply to Surendar V B:

    Hi Surendar,

    Can you share the changes you did in the app.

    Regards,
    Prasad
  • In reply to Prasad Konnur:

    Hi Prasad ,

    I am using mcasp2 pins and I have added pinmux and prcm enable here itself so please find the enclosed code below .

    /******************************************************************************
    **                      INTERNAL MACRO DEFINITIONS
    ******************************************************************************/
    /* Change MACRO DEBUG to 1 in case for checking I2C read and write values */
    #define DEBUG                             (0)

    #define SOC_MCASP_3_FIFO_REGS             (SOC_MCASP2_CFG_BASE + 0x1000)

    /*
    ** Values which are configurable
    */
    /* Slot size to send/receive data */
    #define SLOT_SIZE                         (32U)

    /* Word size to send/receive data. Word size <= Slot size */
    #define WORD_SIZE                         (32U)

    /* Number of channels, L & R */
    #define NUM_I2S_CHANNELS                  (2U)

    /* Number of serializer */
    #define NUM_OF_SERIALIZER                 (1U)

    /* Number of samples to be used per audio buffer */
    #define NUM_SAMPLES_PER_AUDIO_BUF         (96U)

    /* Specify where the parameter set starting is */
    #define PAR_ID_START                      (72U)

    /* McASP Serializer 0 for Transmit */
    #define MCASP_XSER_TX_0                   (0U)

    /*
    ** Below Macros are calculated based on the above inputs
    */
    #define I2S_SLOTS                         ((1 << NUM_I2S_CHANNELS) - 1)

    #define BYTES_PER_SAMPLE                  ((WORD_SIZE >> 3) \
                                               * NUM_OF_SERIALIZER)

    #define AUDIO_BUF_SIZE                    (NUM_SAMPLES_PER_AUDIO_BUF \
                                               * BYTES_PER_SAMPLE)

    #define PAR_TX_START                      (PAR_ID_START)

    /*
    ** EMDA paRAM set size
    */
    #define SIZE_PARAMSET                     (32U)

    /*
    ** Definitions which are configurable depending on the application requirement
    */
    #define MCASP_ACLKX_CLKXDIV_VALUE         (0x6U)
    #define MCASP_AHCLKX_HCLKXDIV_VALUE       (0x9U)

    /*
    ** Audio Codec I2C slave address
    */
    #if defined (SOC_TDA2EX)
    #define AUDIO_CODEC_SLAVE_ADDR            (0x18)
    #else
    /*
     * In case of TDA2xx rev G or higher boards, if SW8 pin 2 is on, the codec
     * address will be 0x19 and if SW8 pin 2 is off, the codec address will be 0x18.
     * On lower version of boards codec address is fixed at 0x18.
     *
     * If the 10 Inch LCD is connected then the address 0x18 conflicts with the
     * STM touch screen. So on Rev G and above use 0x19 as default address for codec
     *
     * To determine the address of codec app will probe 0x19 first, if this fails
     * probe 0x18 for alternate address assuming 10 inch LCD is not connected.
     *
     */
    #define AUDIO_CODEC_SLAVE_ADDR            (0x18)
    #define AUDIO_CODEC_SLAVE_ADDR_1          (0x18)
    #endif

    #define GPIO_IO_EXPANDER_SLAVE_ADDR       (0x26)

    /*
    ** EDMA completion interrupt number
    */
    #define EDMA3_CC_XFER_COMPLETION_INT_A15                (12U)
    #define EDMA3_CC_XFER_COMPLETION_INT_DSP                (38U)

    #ifdef __ARM_ARCH_7A__
    #define EDMA3_CC_XFER_COMPLETION_INT EDMA3_CC_XFER_COMPLETION_INT_A15
    #elif defined _TMS320C6X
    #define EDMA3_CC_XFER_COMPLETION_INT EDMA3_CC_XFER_COMPLETION_INT_DSP
    #endif

    #define INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_MASK     (0x00FF0000U)
    #define INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_SHIFT    (0x00000010U)
    #define INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_RESETVAL (0x00000000U)

    #define INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_MASK     (0x000000FFU)
    #define INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_SHIFT    (0x00000000U)
    #define INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_RESETVAL (0x00000000U)

    #define EDMA3_MAX_CROSS_BAR_EVENTS_TI814X             (230U)

    #define EDMA3_EVENT_MUX_REG_BASE_ADDR                 (0x4a002c78)

    /*:w

    ** Definitions which are configurable depending on the core to be used
    */
    #define EDMA3_CHA_MCASP3_TX               (1)

    #define EDMA3_CC_REGION_A15               (0U)
    #define EDMA3_CC_REGION_DSP               (2U)

    #define EDMA3_CC_QUEUE                    (0U)

    #define MCASP3_RX_DMA_XBAR_INST           (132U)
    #define MCASP3_TX_DMA_XBAR_INST           (133U)

    #define I2S_MODE                          (2U)

    void sampleDelay(int32_t delay);

    /******************************************************************************
    **                      STRUCTURE DEFINITIONS
    ******************************************************************************/
    typedef struct {
        volatile unsigned int TPCC_EVTMUX[32];
    } IntmuxRegs;

    /******************************************************************************
    **                      INTERNAL FUNCTION PROTOTYPES
    ******************************************************************************/
    static void EDMA3IntSetup(void);
    static void I2SDMAParamInit(void);
    static void McASPI2SConfigure(void);
    static void I2SDataTxActivate(void);
    static void EDMA3CCComplIsr(void *dummy);
    void PlatformMCASP3PrcmEnable(void);

    /*I2C Init*/
    void i2c_init(LLD_Hsi2cInstId_t instId);

    /*I2C De-Init*/
    void i2c_deinit();

    LLD_hsi2cErrorCode_t I2CWrite(uint8_t address, uint8_t data);
    LLD_hsi2cErrorCode_t I2CWrite1(uint8_t address, uint8_t data);
    LLD_hsi2cErrorCode_t I2C_Read(uint8_t address, uint8_t *data);
    LLD_hsi2cErrorCode_t I2CWriteBf(uint8_t regAddr, uint8_t bfPosition,
                                    uint8_t bfSize,
                                    uint8_t bfData);

    /*Dac Init*/
    static void aic31InitDac();

    /*Codec Init*/
    static void aic31MdCreateChan();

    static LLD_hsi2cErrorCode_t updateAudioCodecAddr(void);

    /******************************************************************************
    **                      INTERNAL VARIABLE DEFINITIONS
    ******************************************************************************/

    typedef volatile IntmuxRegs *IntmuxRegsOvly;

    /* I2C transfer buffer */
    uint8_t        data_tx[4];

    /* I2C Receive buffer */
    uint8_t        data_rx[4];

    int16_t        _sineWavePattern[] =
    {
        0x0000, 0x0000, 0x10b4, 0x10b4, 0x2120, 0x2120, 0x30fb, 0x30fb, 0x3fff,
        0x3fff, 0x4dea, 0x4dea, 0x5a81, 0x5a81, 0x658b, 0x658b,
        0x6ed8, 0x6ed8, 0x763f, 0x763f, 0x7ba1, 0x7ba1, 0x7ee5, 0x7ee5, 0x7ffd,
        0x7ffd, 0x7ee5, 0x7ee5, 0x7ba1, 0x7ba1, 0x76ef, 0x76ef,
        0x6ed8, 0x6ed8, 0x658b, 0x658b, 0x5a81, 0x5a81, 0x4dea, 0x4dea, 0x3fff,
        0x3fff, 0x30fb, 0x30fb, 0x2120, 0x2120, 0x10b4, 0x10b4,
        0x0000, 0x0000, 0xef4c, 0xef4c, 0xdee0, 0xdee0, 0xcf06, 0xcf06, 0xc002,
        0xc002, 0xb216, 0xb216, 0xa57f, 0xa57f, 0x9a75, 0x9a75,
        0x9128, 0x9128, 0x89c1, 0x89c1, 0x845f, 0x845f, 0x811b, 0x811b, 0x8002,
        0x8002, 0x811b, 0x811b, 0x845f, 0x845f, 0x89c1, 0x89c1,
        0x9128, 0x9128, 0x9a76, 0x9a76, 0xa57f, 0xa57f, 0xb216, 0xb216, 0xc002,
        0xc002, 0xcf06, 0xcf06, 0xdee0, 0xdee0, 0xef4c, 0xef4c
    };

    /*
    ** McASP transmit buffers.
    */
    static uint8_t txBuf0[AUDIO_BUF_SIZE];

    /*
    ** I2C instance zero handle
    */
    hsI2cHandle    i2cHandle;

    /*
    ** I2C instance one handle
    */
    hsI2cHandle    i2cHandle1;

    uint8_t        audioCodecSlaveAddr = (uint8_t) AUDIO_CODEC_SLAVE_ADDR;
    /******************************************************************************
    **                      INTERNAL CONSTATNT DEFINITIONS
    ******************************************************************************/

    /*
    ** Default paRAM for Transmit section. This will be transmitting from
    ** a loop buffer.
    */
    static EDMA3CCPaRAMEntry const txDefaultPar = {
        (uint32_t) EDMA3CC_OPT_TCC_SET(EDMA3_CHA_MCASP3_TX),
        (uint32_t) txBuf0,                                /* source address */
        (uint16_t) (4),                                   /* aCnt */
        (uint16_t) (AUDIO_BUF_SIZE / 4),                  /* bCnt */
        (uint32_t) (SOC_MCASP2_BASE),                     /* dest address */
        (uint16_t) (4),                                   /* source bIdx */
        (uint16_t) (0),                                   /* dest bIdx */
        (uint16_t) (PAR_TX_START * SIZE_PARAMSET),        /* link address */
        (uint16_t) (1),                                   /* bCnt reload value */
        (uint16_t) (0),                                   /* source cIdx */
        (uint16_t) (0),                                   /* dest cIdx */
        (uint16_t) (1)                                    /* cCnt */
    };

    /******************************************************************************
    **                          FUNCTION DEFINITIONS
    ******************************************************************************/

    /* I2C instance Init */
    void i2c_init(LLD_Hsi2cInstId_t instId)
    {
     lld_hsi2c_initParam_t initPar;
     hsI2cObjHandle i2cObjHandle;
     
     initPar.opMode = HSI2C_OPMODE_POLLED;
     initPar.i2cBusFreq = I2C_NORMAL;
     initPar.is10BitAddr = 0;
     initPar.isMasterMode = 1;

     lld_i2c_init(&i2cObjHandle, instId, &initPar);

     if (HSI2C_INST_1 == instId)
     {
     i2cHandle = lld_i2c_open(instId, NULL, NULL);
     }
    #if (defined (SOC_TDA2XX) || defined (SOC_TDA2PX))
     if (HSI2C_INST_1 == instId)
     {
     i2cHandle1 = lld_i2c_open(instId, NULL, NULL);
     }
    #elif (defined (SOC_TDA2EX))
     if (HSI2C_INST_4 == instId)
     {
     i2cHandle1 = lld_i2c_open(instId, NULL, NULL);
     }
    #endif
    }


    /* I2C close and deinit */
    void i2c_deinit()
    {
        lld_i2c_close(&i2cHandle);

        lld_i2c_deinit(HSI2C_INST_0);

        lld_i2c_close(&i2cHandle1);
    #if (defined (SOC_TDA2XX) || defined (SOC_TDA2PX))
        lld_i2c_deinit(HSI2C_INST_1);
    #elif (defined (SOC_TDA2EX))
        lld_i2c_deinit(HSI2C_INST_4);
    #endif
    }

    /* I2C write function */
    LLD_hsi2cErrorCode_t I2CWrite(uint8_t address, uint8_t data)
    {
        LLD_hsi2cErrorCode_t       retVal = LLD_HSI2C_SUCCESS;
        lld_hsi2c_datatfr_params_t i2cXferParams;

        i2cXferParams.bufLen = 2;
        i2cXferParams.buffer = &data_tx[0];

        data_tx[0] = address;
        data_tx[1] = data;

    #if DEBUG
        UARTPuts("\r\n i2c write:   address :  ", -1);
        UARTPutHexNum(data_tx[0]);
        UARTPuts("  data :  ", -1);
        UARTPutHexNum(data_tx[1]);
    #endif

        i2cXferParams.flags = LLD_HSI2C_WRITE | LLD_HSI2C_MASTER | LLD_HSI2C_START
                              | LLD_HSI2C_STOP;
        i2cXferParams.slaveAddr = audioCodecSlaveAddr;
        i2cXferParams.timeout   = 0xFFFFFF;

        retVal = lld_i2c_transfer(i2cHandle, &i2cXferParams);

        if (LLD_HSI2C_SUCCESS != retVal)
        {
            UARTPuts("\r\nI2c write failed ", -1);
        }
    #if DEBUG
        else
        {
            UARTPuts("\r\nI2c write successful ", -1);
        }
    #endif

        return retVal;
    }

    LLD_hsi2cErrorCode_t I2CWrite1(uint8_t address, uint8_t data)
    {
        LLD_hsi2cErrorCode_t       retVal = LLD_HSI2C_SUCCESS;
        lld_hsi2c_datatfr_params_t i2cXferParams;
        hsI2cHandle                ioexpi2cHandle;

        i2cXferParams.bufLen = 2;
        i2cXferParams.buffer = &data_tx[0];

        data_tx[0] = address;
        data_tx[1] = data;

    #if DEBUG
        UARTPuts("\r\n i2c write:   address :  ", -1);
        UARTPutHexNum(data_tx[0]);
        UARTPuts("  data :  ", -1);
        UARTPutHexNum(data_tx[1]);
    #endif

        i2cXferParams.flags = LLD_HSI2C_WRITE | LLD_HSI2C_MASTER | LLD_HSI2C_START
                              | LLD_HSI2C_STOP;
        i2cXferParams.slaveAddr = (uint8_t) GPIO_IO_EXPANDER_SLAVE_ADDR;
        i2cXferParams.timeout   = 0x4000;

    #if defined (SOC_TDA2PX)
        /* For TDA2PX both io expander and the codec are on i2c0 */
        ioexpi2cHandle = i2cHandle;
    #else
        ioexpi2cHandle = i2cHandle1;
    #endif
        retVal = lld_i2c_transfer(ioexpi2cHandle, &i2cXferParams);

        if (LLD_HSI2C_SUCCESS != retVal)
        {
            UARTPuts("\r\nI2c write failed ", -1);
        }
    #if DEBUG
        else
        {
            UARTPuts("\r\nI2c write successful ", -1);
        }
    #endif

        return retVal;
    }

    LLD_hsi2cErrorCode_t I2C_Read(uint8_t address, uint8_t *data)
    {
        LLD_hsi2cErrorCode_t       retVal = LLD_HSI2C_SUCCESS;
        lld_hsi2c_datatfr_params_t i2cXferParams;

        i2cXferParams.bufLen = 1;
        i2cXferParams.buffer = &data_tx[0];

        data_tx[0] = address; /*address byte msb*/

        i2cXferParams.flags =
            LLD_HSI2C_WRITE | LLD_HSI2C_MASTER | LLD_HSI2C_START /*|
                                                                  *LLD_HSI2C_STOP*/;
        i2cXferParams.slaveAddr = audioCodecSlaveAddr;
        i2cXferParams.timeout   = 0xFFFFFF;

        retVal = lld_i2c_transfer(i2cHandle, &i2cXferParams);

        if (LLD_HSI2C_SUCCESS != retVal)
        {
            UARTPuts("\r\nI2c write failed ", -1);
        }
    #if DEBUG
        else
        {
            UARTPuts("\r\nI2c write successful ", -1);
        }
    #endif

        i2cXferParams.buffer = &data_rx[0];
        i2cXferParams.flags  = LLD_HSI2C_READ | LLD_HSI2C_MASTER |
                               LLD_HSI2C_START | LLD_HSI2C_STOP |
                               LLD_HSI2C_IGNORE_BUS_BUSY;
        retVal = lld_i2c_transfer(i2cHandle, &i2cXferParams);

    #if DEBUG
        UARTPuts("\r\n i2c read :   address :  ", -1);
        UARTPutHexNum(data_tx[0]);
        UARTPuts("  data :  ", -1);
        UARTPutHexNum(data_rx[0]);
    #endif

        if (LLD_HSI2C_SUCCESS != retVal)
        {
            UARTPuts("\r\nI2c read failed ", -1);
        }
    #if DEBUG
        else
        {
            UARTPuts("\r\nI2c read successful ", -1);
            *data = data_rx[0];
        }
    #endif

        return retVal;
    }

    LLD_hsi2cErrorCode_t I2CWriteBf(uint8_t regAddr, uint8_t bfPosition,
                                    uint8_t bfSize,
                                    uint8_t bfData)
    {
        uint8_t regData = 0;              /* Temporary Register data      */
        uint8_t mask    = 0;              /* Bit field mask               */
        LLD_hsi2cErrorCode_t retVal = LLD_HSI2C_SUCCESS;

        /*Read data from regAddr*/
        retVal = I2C_Read(regAddr, &regData);

        if (LLD_HSI2C_SUCCESS != retVal)
        {
            UARTPuts("\r\nI2c read failed ", -1);
        }

        mask    = ((1 << bfSize) - 1) << bfPosition;
        regData = (regData & (uint8_t) (~(mask)));
        regData = (regData | (uint8_t) (bfData << bfPosition));

        /* Write the modified data back into the register                 */
        retVal = I2CWrite(regAddr, regData);

        return retVal;
    }

    /**
     *
     *  \brief  This function writes the initialization values for Aic31 DAC
     *          registers. This function should be called to initialize the
     *          registers of the DAC.
     *
     *  \return None
     */
    static void aic31InitDac()
    {
       LLD_hsi2cErrorCode_t retVal = LLD_HSI2C_SUCCESS;
        uint8_t gain = 0x24;

        /* Write the initialization values for the DAC registers                  */
        retVal = I2CWriteBf((uint8_t) Aic31_P0_REG7, (uint8_t) 1, (uint8_t) 4,
                            (uint8_t) 5);

        /* power up the left and right DACs                                       */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG37,
                                             (uint8_t) 0x80));

        /* select the DAC L1 R1 Paths                                             */   //CHANGED FROM 02 TO 01
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG41,
                                             (uint8_t) 0x00));   //00H

        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG42,
                                             (uint8_t) 0x6C));

        /* unmute the DAC                                                         */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG43,
                                             (uint8_t) 0x00));
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG44,
                                             (uint8_t) 0x80));

        /* DAC L to HPL OUT Is connected                                          */  //changed from 47
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG61,
                                             (uint8_t) 0x80));
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG65,
                                             (uint8_t) 0x09));

        /* DAC R to HPROUT is connected                                           */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG64,
                                             (uint8_t) 0x00));
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG65,
                                             (uint8_t) 0x09));

        /* DACL1 connected to LINE1 LOUT                                          */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG82,
                                             (uint8_t) 0x80));
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG86,
                                             (uint8_t) 0x09));

        /* DACR1 connected to LINE1 ROUT                                          */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG89,
                                             (uint8_t) 0x80));
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG93,
                                             (uint8_t) 0x09));

        /* Left/Right DAC digital volume gain                                     */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_LEFT_DAC_VOL_CTRL_ADDR,
                                             /*(uint8_t) gain*/ gain));
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t)
                                             Aic31_RIGHT_DAC_VOL_CTRL_ADDR,
                                             /*(uint8_t) gain*/ gain));

        if (LLD_HSI2C_SUCCESS != retVal)
        {
            //UARTPuts("\r\nDAC Initialization failed ", -1);
        }
        else
        {
            //UARTPuts("\r\nDAC Initialization successful", -1);
        }
    }

    static void aic31MdCreateChan()
    {
      uint8_t tempData            = 0;
        uint8_t pllPValue           = 0;
        uint8_t pllRValue           = 0;
        uint8_t pllJValue           = 0;
        uint8_t pllDLowValue        = 0;
        uint8_t pllDHighValue       = 0;
        uint8_t dualRate            = 0;
        uint8_t sampleRateDiv       = 0;
        uint8_t fsRef               = 0;
        LLD_hsi2cErrorCode_t retVal = LLD_HSI2C_SUCCESS;

        /* Select Register Page 0 of Aic31                            */
        retVal = I2CWrite(Aic31_PAGE_SELECT_ADDR, Aic31_PAGE_0);

        /* Reset the Aic31                                            */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal | I2CWrite(Aic31_P0_REG1, (uint8_t) 0x80));

        /* Configure the audio serial data interface mode             */
        tempData = (0U << 6U);

        /* configure the slot width                                   */
        tempData |= (3U << 4U);

        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite(Aic31_SERIAL_INTERFACEB_ADDR, tempData));

        /* Configure sampleRateDiv and dualRate                        */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG2, (uint8_t) 0,
                                               (uint8_t) 4,
                                               (uint8_t)
                                               sampleRateDiv));

         retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG25, (uint8_t) 6,
                                               (uint8_t) 2,
                                               (uint8_t) 0x11));



        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG7, (uint8_t) 5,
                                               (uint8_t) 1,
                                               (uint8_t) dualRate));

        /* enable the PLL                                             */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG3, (uint8_t) 7,
                                               (uint8_t) 1,
                                               (uint8_t) 1));

        /* select the MCLK as the input for the PLL and CLKDIV(N = 16)*/
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG102,
                                               (uint8_t) 4, (uint8_t) 2,
                                               (uint8_t) 0x00));

        /* select the PLL_IN as codec input                           */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG101,
                                               (uint8_t) 0, (uint8_t) 1,
                                               (uint8_t) 0x00));
    #if 0
        /* selec the GPIO to output the divided PLL_IN clock(test purpose)*/
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG98,
                                            (uint8_t) 0x20));
    #endif

        /* Write to PLL programming register A                            */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG3, (uint8_t) 0,
                                               (uint8_t) 3,
                                               pllPValue));


    //enabled q value as per the datasheet
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG3, (uint8_t) 3,
                                               (uint8_t) 3,
                                               pllPValue));


        /* Write to PLL programming register B                            */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG4, (uint8_t) 2,
                                               (uint8_t) 6,
                                               pllJValue));

        /* write the high and low bits of the D value                     */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal | I2CWrite(Aic31_P0_REG5, pllDHighValue));

        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWrite((uint8_t) Aic31_P0_REG6,
                                             (uint8_t) (pllDLowValue << 2)));

        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG11,
                                               (uint8_t) 0, (uint8_t) 4,
                                               pllRValue));

        /* Write to codec datapath setup register                         */
        retVal =
            (LLD_hsi2cErrorCode_t) (retVal |
                                    I2CWriteBf((uint8_t) Aic31_P0_REG7, (uint8_t) 7,
                                               (uint8_t) 1,
                                               fsRef));

        if (LLD_HSI2C_SUCCESS != retVal)
        {
            //UARTPuts("\r\n Codec Init failed ", -1);
        }
        else
        {
            //UARTPuts("\r\n Codec Init successful ", -1);
        }

        /* Initialize DAC*/
        aic31InitDac();
    }

    /*
    ** Initializes the DMA parameters.
    ** The TX basic paRAM set (channel) is 12.
    **
    ** The TX paRAM sets will be initialized to transmit from the loop buffer.
    ** The size of the loop buffer can be configured.
    ** The transfer completion interrupt will not be enabled for paRAM set 1;
    ** paRAM set 1 will be linked to linked paRAM set starting (PAR_TX_START) of TX.
    ** All other paRAM sets will be linked to itself.
    ** and further transmission only happens via linked paRAM set.
    ** For example, if the PAR_TX_START value is 72, and the number of paRAMS is 2,
    ** So transmission paRAM set linking will be initialized as 1-->72-->73, 73->73.
    */
    static void I2SDMAParamInit(void)
    {
        int16_t          *sineToneDataPtr = NULL;
        int32_t          *temp;
        uint32_t          i = 0;
        EDMA3CCPaRAMEntry paramSet;

        /* Initialize TX Buffers
         *
         * These patterns are seen/output on serializer0 and serializer1
         */

        sineToneDataPtr = _sineWavePattern;

        temp = (int32_t *) txBuf0;

        for (i = 0; i < (AUDIO_BUF_SIZE / 4); i++)
        {
            *temp = (int32_t) (*sineToneDataPtr);

            temp++;
            sineToneDataPtr++;
        }

        /* Initialize the 1st paRAM set for transmit */
        memcpy(&paramSet, &txDefaultPar, SIZE_PARAMSET - 2);

        EDMA3SetPaRAM(SOC_EDMA_TPCC_BASE_VIRT, EDMA3_CHA_MCASP3_TX, &paramSet);

        /*Set Link parameters*/
        EDMA3SetPaRAM(SOC_EDMA_TPCC_BASE_VIRT, PAR_TX_START, &paramSet);
    }

    /*
    ** Configures the McASP Transmit Section in I2S mode.
    */
    static void McASPI2SConfigure(void)
    {
        McASPTxReset(SOC_MCASP2_CFG_BASE);

        /* Enable the FIFOs for DMA transfer */
        McASPWriteFifoEnable(SOC_MCASP_3_FIFO_REGS, 1, 1);

        /* Set the mask assuming integer format for 32 bit word*/
        McASPTxFmtMaskSet(SOC_MCASP2_CFG_BASE, 0xFFFFFFFF);

        /* Set I2S format in the transmitter/receiver format units */
        McASPTxFmtSet(SOC_MCASP2_CFG_BASE, (MCASP_TX_SYNC_DELAY_0BIT |
                                            MCASP_TX_BITSTREAM_MSB_FIRST |
                                            MCASP_TX_SLOTSIZE_32BITS |
                                            MCASP_TX_ROT_RIGHT_20BITS));

        McASPTxFrameSyncCfg(SOC_MCASP2_CFG_BASE, I2S_MODE, MCASP_TX_FS_WIDTH_WORD,
                            MCASP_TX_FS_EXT_BEGIN_ON_FALL_EDGE |
                            MCASP_TX_FS_INTERNAL);

        /* configure the clock for transmitter */
        McASPTxClkCfg(SOC_MCASP2_CFG_BASE, MCASP_TX_CLK_INTERNAL,
                      ((MCASP_ACLKX_CLKXDIV_VALUE & MCASP_ACLKXCTL_CLKXDIV_MASK) >>
                       MCASP_ACLKXCTL_CLKXDIV_SHIFT),
                      ((MCASP_AHCLKX_HCLKXDIV_VALUE &
                        MCASP_AHCLKXCTL_HCLKXDIV_MASK) >>
                       MCASP_AHCLKXCTL_HCLKXDIV_SHIFT));

        McASPTxClkPolaritySet(SOC_MCASP2_CFG_BASE, MCASP_TX_CLK_POL_FALL_EDGE);

        McASPTxClkCheckConfig(SOC_MCASP2_CFG_BASE, MCASP_TX_CLKCHCK_DIV32, 0x00,
                              0xFF);

        /* Enable the transmitter/receiver slots. I2S uses 2 slots */
        McASPTxTimeSlotSet(SOC_MCASP2_CFG_BASE, I2S_SLOTS);

        /*
        ** Set the serializers
        */
        McASPSerializerTxSet(SOC_MCASP2_CFG_BASE, MCASP_XSER_TX_0);

        /*
        ** Configure the McASP pins
        ** Output - Frame Sync, Clock, Serializer Rx and Serializer Tx
        **          (Clocks generated internally)
        */
        McASPPinMcASPSet(SOC_MCASP2_CFG_BASE,
                         (MCASP_PIN_AFSX
                          | MCASP_PIN_AHCLKX | MCASP_PIN_ACLKX | MCASP_PIN_AMUTE
                          | MCASP_PIN_AXR(MCASP_XSER_TX_0)
                         ));

        McASPPinDirOutputSet(SOC_MCASP2_CFG_BASE, MCASP_PIN_AFSR);
        McASPPinDirOutputSet(SOC_MCASP2_CFG_BASE, MCASP_PIN_ACLKR);

        McASPPinDirOutputSet(SOC_MCASP2_CFG_BASE, MCASP_PIN_AFSX);

        /* Configure high clock as Output */
        McASPPinDirOutputSet(SOC_MCASP2_CFG_BASE, MCASP_PIN_AHCLKX);

        McASPPinDirOutputSet(SOC_MCASP2_CFG_BASE, MCASP_PIN_ACLKX);

        /* Both Serializers used to output data out */
        McASPPinDirOutputSet(SOC_MCASP2_CFG_BASE, MCASP_PIN_AXR(MCASP_XSER_TX_0));
    }

    /*
    ** Sets up the interrupts for EDMA in AINTC
    */
    static void EDMA3IntSetup(void)
    {
        /*Unlock the Crossbar register */
        PlatformUnlockMMR();

    #ifdef __ARM_ARCH_7A__
        IRQXBARConnect(SOC_IRQ_DMARQ_CROSSBAR_REGISTERS_BASE, CPU_MPUSS, 7,
                       EDMA_TPCC_IRQ_REGION0);

    #elif defined (_TMS320C6X)
        IRQXBARConnect(SOC_IRQ_DMARQ_CROSSBAR_REGISTERS_BASE, CPU_DSP1, 7,
                       EDMA_TPCC_IRQ_REGION2);
    #endif

        /* Enable The EDMA interrupt */
        Intc_Init();
        Intc_IntEnable(0);

        Intc_IntRegister(EDMA3_CC_XFER_COMPLETION_INT,
                         (IntrFuncPtr) EDMA3CCComplIsr,
                         NULL);
        Intc_IntPrioritySet(EDMA3_CC_XFER_COMPLETION_INT, 1, 0);
        Intc_SystemEnable(EDMA3_CC_XFER_COMPLETION_INT);
    }

    /*
    ** Activates the data transmission/reception
    ** The DMA parameters shall be ready before calling this function.
    */
    static void I2SDataTxActivate(void)
    {

            
        /* Start the clocks */
        McASPTxClkStart(SOC_MCASP2_CFG_BASE, MCASP_TX_CLK_INTERNAL);


    #if 1

        /* Enable EDMA for the transfer */
        EDMA3EnableTransfer(SOC_EDMA_TPCC_BASE_VIRT, EDMA3_CHA_MCASP3_TX,
                            EDMA3_TRIG_MODE_EVENT);
        


        /* Activate the  serializers */
        McASPTxSerActivate(SOC_MCASP2_CFG_BASE);
        

        /* make sure that the XDATA bit is cleared to zero */
       while (McASPTxStatusGet(SOC_MCASP2_CFG_BASE) & MCASP_TX_STAT_DATAREADY) ;

        

        /* Activate the state machines */



     
           McASPTxEnable(SOC_MCASP2_CFG_BASE);

    #endif
    }

    void sampleConfigScr(unsigned int eventNum, unsigned int chanNum) {
        unsigned int   scrChanOffset = 0;
        unsigned int   scrRegOffset  = 0;
        unsigned int   xBarEvtNum    = 0;
        IntmuxRegsOvly scrEvtMux     =
            (IntmuxRegsOvly) (EDMA3_EVENT_MUX_REG_BASE_ADDR);

        if ((eventNum < EDMA3_MAX_CROSS_BAR_EVENTS_TI814X) &&
            (chanNum < EDMA3_NUM_TCC))
        {
            scrRegOffset  = chanNum / 2;
            scrChanOffset = chanNum - (scrRegOffset * 2);
            xBarEvtNum    = (eventNum + 1);

            switch (scrChanOffset)
            {
                case 0:
                    scrEvtMux->TPCC_EVTMUX[scrRegOffset] &=
                        ~(INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_MASK);
                    scrEvtMux->TPCC_EVTMUX[scrRegOffset] |=
                        (xBarEvtNum & INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_MASK);
                    break;
                case 1:
                    scrEvtMux->TPCC_EVTMUX[scrRegOffset] &=
                        ~(INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_MASK);
                    scrEvtMux->TPCC_EVTMUX[scrRegOffset] |=
                        ((xBarEvtNum <<
                          INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_SHIFT) &
                         (INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_MASK));
                    break;
                default:
                    break;
            }
        }
    }

    /*Configure EDMA Xbar*/
    void Configure_Edma_xbar()
    {
        sampleConfigScr(MCASP3_RX_DMA_XBAR_INST, EDMA3_CHA_MCASP3_TX);
    }

    /*Pin Mux and Clk config*/
    void pinMuxClkConfig(void)
    {
        /*Unlock the Control registers */
        PlatformUnlockMMR();

        /* Pad mux configuration for McASP instance 2 */
        PlatformMCASP3SetPinMux();

        /* Power on McASP instance 2*/
        PlatformMCASP3PrcmEnable();
    #if (defined (SOC_TDA2XX) || defined (SOC_TDA2PX))
        /* Pad mux configuration for I2C instance 2 */
        PlatformI2C2SetPinMux();
    #elif (defined (SOC_TDA2EX))
        /* Pad mux configuration for I2C instance 5 */
        PlatformI2C5SetPinMux();
    #endif

        PlatformUART1SetPinMux();
    }

    /*Edma Config*/
    void edmaConfig(void)
    {
    #if defined (__ARM_ARCH_7A__)
        EDMAsetRegion(EDMA3_CC_REGION_A15);
    #elif defined (_TMS320C6X)
        EDMAsetRegion(EDMA3_CC_REGION_DSP);
    #endif

        EDMA3Init(SOC_EDMA_TPCC_BASE_VIRT, EDMA3_CC_QUEUE);

        Configure_Edma_xbar();

        EDMA3IntSetup();

        /* Request EDMA channels */
        EDMA3RequestChannel(SOC_EDMA_TPCC_BASE_VIRT, EDMA3_CHANNEL_TYPE_DMA,
                            EDMA3_CHA_MCASP3_TX, EDMA3_CHA_MCASP3_TX,
                            EDMA3_CC_QUEUE);
    }

    static LLD_hsi2cErrorCode_t updateAudioCodecAddr(void)
    {
        LLD_hsi2cErrorCode_t retVal = LLD_HSI2C_SUCCESS;

        //UInt32 i2cInstId1 = 1;
        retVal = lld_i2c_probe(i2cHandle, 0x18);
        if (LLD_HSI2C_SUCCESS != retVal)
        {
    #ifdef AUDIO_CODEC_SLAVE_ADDR_1
            retVal = lld_i2c_probe(i2cHandle, 0x18);
            if (LLD_HSI2C_SUCCESS != retVal)
            {
                UARTPuts("\r\nProbe to audio codec failed ", -1);
                retVal = LLD_HSI2C_FAIL;
            }
            else
            {
                /* Use the Alternate Audio Codec Addr */
                audioCodecSlaveAddr = AUDIO_CODEC_SLAVE_ADDR_1;
            }
    #else
            UARTPuts("\r\nProbe to audio codec failed ", -1);
            retVal = LLD_HSI2C_FAIL;

    #endif
        }
        else
        {
            /* Use the default Audio Codec Addr */
            audioCodecSlaveAddr = AUDIO_CODEC_SLAVE_ADDR;
        }

        return retVal;
    }

    /*:W

    ** The
    ** main function. Application starts here.
    */
    int main(void)
    {

        sampleDelay(5000);

        UARTStdioInit();

        UARTPuts("\r\nMcASP Sinetone application ", -1);


        uint32_t value = HW_RD_REG32(SOC_MCASP2_CFG_BASE);
        UARTPutHexNum(value);

        LLD_hsi2cErrorCode_t retVal = LLD_HSI2C_SUCCESS;

        /*Pin Mux and Clk config*/
            pinMuxClkConfig();


        /*I2C instance 0 init*/
        //i2c_init(HSI2C_INST_0);
        i2c_init(HSI2C_INST_1);


        retVal = updateAudioCodecAddr();
        if (LLD_HSI2C_SUCCESS != retVal)
        {
         UARTPuts("\r\ninside update audio codec addr ", -1);
            /* Cannot Probe the audio codec */
            while (1) ;
        }

        /*Edma Config*/
        edmaConfig();

        /*Init Codec and DAC*/
        aic31MdCreateChan();

        /* Initialize the DMA parameters */
        I2SDMAParamInit();


        /* Configure the McASP*/
        McASPI2SConfigure();


        /* Activate the audio transmission and reception */
        I2SDataTxActivate();


        /*De-initialize I2C*/
        i2c_deinit();


        /* Data Transfer happens infinitely even though application ends
         * here. Removed while loop as compiler issues warning of non
         * returnable main function
         */
        return 0;
    }

    /*
    ** EDMA transfer completion ISR
    */
    static void EDMA3CCComplIsr(void *dummy)
    {
        /* Check if transmit DMA completed */
        if (EDMA3GetIntrStatus(SOC_EDMA_TPCC_BASE_VIRT) & (1 << EDMA3_CHA_MCASP3_TX))
        {
            /* Clear the interrupt status for the first channel */
            EDMA3ClrIntr(SOC_EDMA_TPCC_BASE_VIRT, EDMA3_CHA_MCASP3_TX);
        }
    }

    void PlatformMCASP3SetPinMux(void)
    {
            /*AUDIO*/
            /*Pad configuration*/
        #define CTRL_CORE_SEC_SMA_SW_14 (0x290U)      
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE + CTRL_CORE_PAD_IO_GPMC_AD7, 0x0000000F);
            HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE + CTRL_CORE_PAD_IO_GPMC_AD5, 0x0000000F);
            HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE + CTRL_CORE_PAD_IO_GPMC_AD6, 0x0000000F);
            HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE + CTRL_CORE_PAD_IO_GPMC_AD10, 0x0000000F);
            HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE + CTRL_CORE_PAD_IO_GPMC_AD11, 0x0000000F);
            HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE + CTRL_CORE_PAD_IO_GPMC_BEN0, 0x0006000E);
                    
        GPIODirModeSet(SOC_GPIO1_BASE, 1, GPIO_DIR_OUTPUT);
        GPIOPinWrite(SOC_GPIO1_BASE, 1, GPIO_PIN_HIGH);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE + CTRL_CORE_PAD_IO_GPMC_BEN1, 0x0006000E); //AUDIO SPEAKER ENABLE
        GPIODirModeSet(SOC_GPIO1_BASE, 2, GPIO_DIR_OUTPUT);
        GPIOPinWrite(SOC_GPIO1_BASE, 2, GPIO_PIN_HIGH);
        
        HW_WR_REG32(SOC_SEC_EFUSE_REGISTERS_BASE + CTRL_CORE_SEC_SMA_SW_14, 0x00200033);
    /**  FOR LOOPBACK
        HW_WR_FIELD32(SOC_MCASP2_CFG_BASE + MCASP_LBCTL, MCASP_LBCTL_DLBEN,
                                  MCASP_LBCTL_DLBEN_ENABLE);
        HW_WR_FIELD32(SOC_MCASP2_CFG_BASE + MCASP_LBCTL, MCASP_LBCTL_IOLBEN,
                                  MCASP_LBCTL_IOLBEN_ENABLE);
        HW_WR_FIELD32(SOC_MCASP2_CFG_BASE + MCASP_LBCTL, MCASP_LBCTL_MODE,
                                  MCASP_LBCTL_MODE_XMTCLK);
        HW_WR_FIELD32(SOC_MCASP2_CFG_BASE + MCASP_LBCTL, MCASP_LBCTL_ORD, 0x0);
        HW_WR_FIELD32( SOC_MCASP2_CFG_BASE + MCASP_ACLKXCTL,
                    MCASP_ACLKXCTL_ASYNC,
                    MCASP_ACLKXCTL_ASYNC_SYNC);

        HW_WR_REG32(SOC_MCASP2_CFG_BASE + MCASP_TXFMCTL,0x00000200);

        HW_WR_REG32(SOC_MCASP2_CFG_BASE + MCASP_RXFMCTL,0x00000200);**/
        
    }



    void PlatformMCASP3PrcmEnable(void)
    {
        HW_WR_REG32(0x4a009860, 0x02);
        while ((HW_RD_REG32(0x4a009860)) != 0x02U)
        {
            ;
        }
    }


    void sampleDelay(int32_t delay)
    {
        volatile int32_t i, j;

        for (i = 0; i < delay; i++)
        {
            for (j = 0; j < 100; j++) ;
        }
    }

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.