This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

EVMK2H: A question about EVMK2H boot modes

Part Number: EVMK2H

Hi 

Recently I bought the EVMK2H and can run some simple project which I ran on 6678 before like Client, Hello world and Image Processing.

Now I faced with some problems that confused me. I use these softwares:

CCS v7.4.0

processor_sdk_rtos_k2hk_4_03_00_05 

mcsdk_bios_3_01_04_07

my qustions:

1. What is the differences between mcsdk and processor_sdk_rtos? 

2. How can I build Bin file for EEPROM, SPI and Ethernet boot mode for DSP and ARM(single stage or multi stage)? I know I should use C6000 and ARM code generation tools but I don't know how should I convert and which tools I should use for each boot mode.

3. Can I compile all projects even ARM on windows or I must use linux? for example if I want to change and build u-boot and program it, have to use linux os?

4. for now my target is building the Matrix project and load as u-boot on SPI flash. But I don't know where can I find this project and how I should compile and make bin file for SPI.

If you can introduce me any tread which can help, I will be appreciate. 

Thanks

  • In reply to alireza zakani:

    Dear Alireza
    Now I have power failure problem in my board and can not do any test. Please inform me if you found any solutions.
    Thanks
  • Guru 80755 points

    In reply to patrick NA:

    Hi ,

    Please refer below post from Rahul for boot procedure and boot image generation.

    Thank you.

    Regards,
    Rajasekaran K
    -----------------------------------------------------------------------------------------------------------
    Don't forget to click the Verify Answer button if this post answers your question.
    PLEASE READ FIRST: Keystone I & II Multicore Forum Usage Guidelines
    Learn More About Keystone Multicore Devices: Resources for Keystone Devices

    Please download the latest Processor SDK for Keystone I & II devices(C665x, C667x, K2H, K2E, k2G & K2L).

  • In reply to Raja:

    Hi dear Raja
    Your helps always are useful. I faced with "SOC Power Failure" problem in my EVM and even programming UCDs or BMC was not effective. I bring it up in the below post.
    e2e.ti.com/.../2612575
    Please help me if you can till solve it.
    Thanks.
  • In reply to patrick NA:

    Hi Patrick,

    I am aware of your other thread and I think you're facing a hw problem, which is not related to the boot procedure. If you're trying to boot the same board through SPI boot, then you need to fix your hw issue first.
    I've escalated the other thread to the hw designers, wait for their feedback.

    I am closing this thread for now.

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Thanks a lot. I will wait for your good helps. Truly the board stopped suddenly and I did nothing.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.