This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Connecting XDS510PP - Plus to CCS v3.3

Expert 1440 points

Replies: 2

Views: 1341

 

Hi,

I am using CCS 3.3 and trying to connect my XDS510PP-Plus emulator.

The emulator connection isgood, I verified it by running the SDConfig utility by

Spectrum Digital. It can do emulator rest, verify and Test (it gives 2 JTAG devices connected).

When I open the CCS and try to connect the device (Debug -> Connect), I get the following error.

Can somebody tell me how to get rid of the error and if I am missing any drivers files?

 

Error connecting to the target:
Error 0x80001240/-1062
Fatal Error during: Initialization, OCS, Target,
Device driver: Power Loss Detected on Target CPU.
This could also result from disconnecting the emulator from the target.
It is recommended to RESET EMULATOR.  This will disconnect each
target from the emulator.  The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.


Sequence ID: 0
Error Code: -1062
Error Class: 0x80001240
I/O Port = 378

Board Name: C5510 v2 PP Emulator
Cpu Name: c5510

Abort:        Close Code Composer Studio.
Retry:        Try to connect to the target again.
Cancel:        Remain disconnected from the target
Diagnostic:    Run diagnostic utility.

 

Thanks,

Regards,

Aditi.

  • Hi Aditi,

    Spectrum Digital has a support website. Have you completed their Installation Instructions for CCStudio v3.3 and the Spectrum Digital XDS510 USB/PP+ JTAG Emulator?

    http://support.spectrumdigital.com/ccs33/

    Hope this helps,
    Mark

  • In reply to Mark Mckeown:

    Hi,

    Thank you for all the suggestion. I have fixed the problem.

    I had a bad oscillator on my module which did not supply clock to the DSP.

     

    Regards,

    Aditi.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.