This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

M4 IPU Cache Enabling TIMER2 Hard_FAULT

Intellectual 700 points

Replies: 18

Views: 571

Hi,

directly after enabling the cache with UNICACHEEnable(SOC_IPU1_UNICACHE_MMU_CONF_REGS_BASE) I configure the GP-Timer2.

If I don't insert a wait loop after cache enabling I get a HARD_FAULT.

Do I need to wait after cache enabling or what else could it be?

Thanks

Andreas

  • Hi Andreas,

    Can you provide more details on the scenario where you are getting hard fault like AMMU config, memory where you are running. etc.

    Regards,
    Rishabh
  • In reply to Rishabh Garg:

    Hi Rishabh,

    It happens during TIMERReset() function. The code is running on DDR RAM 0x9E000000.

    The structure is like this:

       UNICACHEEnable()
    
       for(uint32_t x = 0;x < 9999999; x++)
       {
          __asm__("nop");
       }
    
        TIMERReset()
    

    Do I need some wait time?

    Regards,

    Andreas

  • In reply to Andreas Vogt57:

    Hi Andreas,

    You don't need any wait after enabling cache.
    Ideally you should not have faced this issue, most probably some sequence is not absolutely correct in the system context.

    As a workaround can you add UNICACHEInvalidateAll after enabling cache and try.

    Regards,
    Rishabh
  • In reply to Rishabh Garg:

    Hi,

    I have the following message when TimerReset() is triggered:

    [ 10.512559] WARNING: CPU: 0 PID: 0 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x23c/0x368()
    [ 10.512581] 44000000.ocp:L3 Custom Error: MASTER IPU1 TARGET L4_PER1_P3 (Read): Data Access in User mode during Functional access
    [ 10.512595] Modules linked in:
    [ 10.512624] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.4.84-SMS_MONOLYTHIC-svn36 #25
    [ 10.512640] Hardware name: Generic DRA74X (Flattened Device Tree)
    [ 10.512654] Backtrace:
    [ 10.512695] [<c0012f6c>] (dump_backtrace) from [<c0013108>] (show_stack+0x18/0x1c)
    [ 10.512710] r6:20000193 r5:ffffffff r4:00000000 r3:00000000
    [ 10.512765] [<c00130f0>] (show_stack) from [<c029804c>] (dump_stack+0x88/0xa8)
    [ 10.512789] [<c0297fc4>] (dump_stack) from [<c0041844>] (warn_slowpath_common+0x80/0xbc)
    [ 10.512802] r8:c075d670 r7:00000009 r6:00000093 r5:c02c88f8 r4:c081bd60 r3:c081a000
    [ 10.512859] [<c00417c4>] (warn_slowpath_common) from [<c0041924>] (warn_slowpath_fmt+0x38/0x40)
    [ 10.512872] r8:c060ab34 r7:c075d8b4 r6:eee0d910 r5:c075d5cc r4:80080003
    [ 10.512924] [<c00418f0>] (warn_slowpath_fmt) from [<c02c88f8>] (l3_interrupt_handler+0x23c/0x368)
    [ 10.512937] r3:eee0d780 r2:c075d68c
    [ 10.512970] [<c02c86bc>] (l3_interrupt_handler) from [<c0089dec>] (handle_irq_event_percpu+0x64/0x164)
    [ 10.512984] r10:eedfa240 r9:c086d6fa r8:00000017 r7:00000000 r6:00000000 r5:eedfa2a0
    [ 10.513030] r4:eee0dc80
    [ 10.513055] [<c0089d88>] (handle_irq_event_percpu) from [<c0089f2c>] (handle_irq_event+0x40/0x64)
    [ 10.513068] r10:c081bf10 r9:eec08000 r8:00000001 r7:00000000 r6:c082766c r5:eedfa2a0
    [ 10.513112] r4:eedfa240
    [ 10.513137] [<c0089eec>] (handle_irq_event) from [<c008d0f8>] (handle_fasteoi_irq+0xe4/0x1ac)
    [ 10.513150] r6:c082766c r5:eedfa2a0 r4:eedfa240 r3:00000000
    [ 10.513194] [<c008d014>] (handle_fasteoi_irq) from [<c008961c>] (generic_handle_irq+0x20/0x30)
    [ 10.513206] r7:00000000 r6:c08163fc r5:00000017 r4:c08163fc
    [ 10.513248] [<c00895fc>] (generic_handle_irq) from [<c008975c>] (__handle_domain_irq+0x70/0xec)
    [ 10.513269] [<c00896ec>] (__handle_domain_irq) from [<c0009504>] (gic_handle_irq+0x40/0x84)
    [ 10.513281] r10:00000000 r9:00000000 r8:fa213000 r7:fa212000 r6:c081bf10 r5:c081d948
    [ 10.513326] r4:fa21200c r3:c081bf10
    [ 10.513356] [<c00094c4>] (gic_handle_irq) from [<c0013c74>] (__irq_svc+0x54/0x90)
    [ 10.513371] Exception stack(0xc081bf10 to 0xc081bf58)
    [ 10.513389] bf00: 00000001 00000000 00000000 fe600000
    [ 10.513412] bf20: c05d322c 00000000 c0817558 c0815364 00000001 00000000 c081d56c c081bf6c
    [ 10.513431] bf40: c081bf4c c081bf60 c0034f74 c001073c 60000013 ffffffff
    [ 10.513444] r10:c081d56c r8:00000001 r7:c081bf44 r6:ffffffff r5:60000013 r4:c001073c
    [ 10.513504] [<c0010718>] (arch_cpu_idle) from [<c007c65c>] (default_idle_call+0x28/0x34)
    [ 10.513526] [<c007c634>] (default_idle_call) from [<c007c7b8>] (cpu_startup_entry+0x150/0x27c)
    [ 10.513549] [<c007c668>] (cpu_startup_entry) from [<c05ca0d8>] (rest_init+0x7c/0x94)
    [ 10.513561] r7:c0870000
    [ 10.513587] [<c05ca05c>] (rest_init) from [<c07cacc8>] (start_kernel+0x368/0x3e0)
    [ 10.513599] r4:c0870040 r3:c081a000
    [ 10.513630] [<c07ca960>] (start_kernel) from [<8000807c>] (0x8000807c)
    [ 10.513644] ---[ end trace b0aa3858056ad469 ]---

  • In reply to Andreas Vogt57:

    Hi,

    UNICACHEInvalidateAll seems to work. Do you have an idea why?

    Thanks
    Andreas
  • In reply to Andreas Vogt57:

    Hi Andreas,

    It is working as the cache was not in a clean state when you enabled.
    Invalidate made it clean.

    Regards,
    Rishabh
  • In reply to Rishabh Garg:

    Hi,

    sorry after some testing I have to tell that the problem is still there.
    I am quite sure that Linux is not using GP-Timers.
    And Timer1 I can reset without a problem. Timer 2/3/4 cause hard fault.

    Andreas
  • In reply to Andreas Vogt57:

    Hi Andreas,

    Did you check if the Timer2/3/4 were running when you tried to reset?

    Regards,
    Rishabh
  • In reply to Rishabh Garg:

    Hi,

    I checked the registers and I saw that if I enable TIMER2 (MODULEMODE = 0x2) before TimerReset(), the register 0x4a009738 is equal to 0x00020002 which says  "0x2: Module is in Idle mode (only OCP part). It is functional if using separate functional clock". But it should be "0x0: Module is fully functional, including OCP" ,right?

    What does OCP means? 

    Regards

    Andreas

  • In reply to Andreas Vogt57:

    Hi Andreas,

    This means you are trying to access Timer2 registers when Timer2 is off.
    May I know what exactly do you want achieve?
    OCP is protocol for communication used by hardware. You can search internet for details.

    Regards,
    Rishabh

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.