This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Announce: Very Fast Boot (0.5 sec)

Expert 2995 points

Replies: 5

Views: 11624

I am pleased to announce very fast boot for dm365.
It takes 0.5 (half of a second) from kernel initialization (not including u-boot and kernel unzip) till command line prompt.

Download ready uImage with root FS and test it: http://www.makelinux.net/ti/fastboot/

Boot time measured by printing  /proc/uptime from boot script.

Solution:

  • Linux kernel 2.6.18 from MontaVista Linux 5
  • minimal kernel configuration with some source code tuning. Kernel configuration located in /proc/config.gz
  • Root FS implemented with Busybox and connected as Init RAM FS and included in uImage. Busybox configuration located in /etc/busybox.config

Enjoy.

See also: Booting Linux dm365 Network Camera in 3.2 seconds


Constantine
Embedded Linux Consulting: http://www.MakeLinux.com/
Linux and TI DaVinci Technology Portal: http://www.Linux-DaVinci.info/

Please consider to   Verify the Answer   if applicable

  • Hello All,

    When I burned ubl and uboot on nand flash with small block size (hynix 64MB) using DM35x_FlashAndBootUtils_1_50 through serial port, I got error message "No good blocks in allowed range". I used a new nand flash. So please tell me it is why. thanks a lot.

    Best Regards,

    Mark

  • In reply to YHLShareware:

    @Mark/ - you probably posted to the wrong topic.

     

    on topic: nice value - according to the wiki there were already several efforts (total boot in less than 1s) in speeding kernel boot up. the overall value from power on until the user can launch its application is in fact the more interesting one. (and its as well dependent on the size of the kernel image to load and unpack, so a sole linux kernel boot value does not tell anything)

  • In reply to Alexander Stohr:

    Thanks.

    Time of loading kernel from flash depends from flash type NAND/NOR, throughput, UBL/u-boot configuration and eventually kernel and FS size.


    Constantine
    Embedded Linux Consulting: http://www.MakeLinux.com/
    Linux and TI DaVinci Technology Portal: http://www.Linux-DaVinci.info/

    Please consider to   Verify the Answer   if applicable

  • Please read update:  Booting Linux dm365 Network Camera in 3.2 seconds


    Constantine
    Embedded Linux Consulting: http://www.MakeLinux.com/
    Linux and TI DaVinci Technology Portal: http://www.Linux-DaVinci.info/

    Please consider to   Verify the Answer   if applicable

  • In reply to Constantine:

    i  want to make a nfs file with busybox1.13.3 on platform DM365.but it can not run the /sbin/init.

    if  i replace the /sbin/init with the montavista/nfs/sbin/init,it is right.

    my cross_compile of busybox  is arm-linux-gcc3.3.2.

    and my kernel  is arm_v5t_le-gcc.

    can you tell me why the busybox/sbin/init can not run.

    is it the compiler can not match?

    and can you tell which kind of busbox should i use to make?

    thx

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.