This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/66AK2H12: Cannot find Hello World example project for K2H EVM

Prodigy 130 points

Replies: 12

Views: 472

Part Number: 66AK2H12

Tool/software: Code Composer Studio

Hi there,

I want to get a simple Hello World example working with the 66AK2H12 (K2H EVM), I'm following the guide here: http://processors.wiki.ti.com/index.php/Processor_SDK_Bare_Metal_Examples#ARM_Cortex-A15  

1. Start CCS and create a work space for generating the project.

Fine, no problem.

2. Click on File menu option and select New--> CCS Project.

Fine, no problem.

3. Select Target as AM572x -Cortex A15 and GPEVM_AM572x as shown in the image

Fine - I switched the target to my own board's settings

4. Select Cortex A setting in the options below and provide name of the project as "hello_world" and use default Advanced settings for the project. If the Default settings uses "TI ARM compiler 5.x.x" switch to GNU Linaro 4.8.4 (or higher) tool chain for A15 and check the build little endian ELF binary for the A15 core. Under Project templates and examples, select Basic Examples-> Hello World

Click Finish after you are done to allow CCS to auto generate the project from the template Basic Examples-> Hello World.

Here is the problem. I cannot find Basic Examples -> Hello World. 

 


Basic Examples -> Hello World doesn't exist within my CCS install. How can I get this example project? I checked the Resource Explorer, and I can't find a way to download anything called Hello World.

 

Thanks for any help!

  • In reply to Rahul Prabhu:

    Rahul,

    Why would I end my program with a while(1)? Wouldn't that keep my program from terminating? I'm not sure I'm following...

    Also how can I put the core in WFI (Wait For Interrupt)?

    Thanks,

    Andre

  • Guru 81165 points

    In reply to Andre B37:

    Also how can I put the core in WFI (Wait For Interrupt)?

    __wfi();

    Regards,
    Rajasekaran K
    -----------------------------------------------------------------------------------------------------------
    Don't forget to click the Verify Answer button if this post answers your question.
    PLEASE READ FIRST: Keystone I & II Multicore Forum Usage Guidelines
    Learn More About Keystone Multicore Devices: Resources for Keystone Devices

    Please download the latest Processor SDK for Keystone I & II devices(C665x, C667x, K2H, K2E, k2G & K2L).

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.