This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

RTOS/AM3352: Ping fails in NIMU basic example project

Intellectual 810 points

Replies: 13

Views: 375

Part Number: AM3352

Tool/software: TI-RTOS

Hi

     when I use the default project NIMU_BasicExample_bbbAM335x_armExampleproject for my test,

I can't ping the device successful.

Through the code, we learned that the code related to the initialization of emac has the following parts:

/* Chip configuration MII/RMII selection */
SOCCtrlCpswPortMacModeSelect(1, ETHERNET_MAC_TYPE_RMII);
SOCCtrlCpswPortMacModeSelect(0, ETHERNET_MAC_TYPE_RMII);

EMAC_socGetInitCfg(0, &cfg);
cfg.port[0].phy_addr = EMAC_CPSW_PORT0_PHY_ADDR_EVM;
cfg.port[1].phy_addr = EMAC_CPSW_PORT0_PHY_ADDR_EVM;
cfg.macModeFlags = EMAC_CPSW_CONFIG_MODEFLG_FULLDUPLEX;
EMAC_socSetInitCfg(0, &cfg);

/create app task/

NIMUDeviceTable[nimu_device_index++].init = &CpswEmacInit ;
NIMUDeviceTable[nimu_device_index].init = NULL ;

about the soc,is there any config for HW except SOCCtrlCpswPortMacModeSelect?

and I know the init and register EMAC is by CpswEmacInit .

how can I know init and register EMAC success,is there any log?

I don't know how does CpswEmacInit  function exectued.so I don't know if EMAC has init or register.

BR!

  • Guru 67150 points
    Hi,

    Did you use the latest Processor SDK RTOS for AM335x (5.3 release) for testing? All the software examples are verified via system test before release. So I expect the NIMU_BasicExample_bbbAM335x_armExampleproject should work as it is. Let me know if 5.3 release worked for you or not. If not, I will find a BBB to test.

    Regards, Eric
  • In reply to lding:

    Hi

        my PDK version is 5.2,I have do many work for my project.so I don't want to update to 5.3,

    I think there are some errors on the EMAC configure,can you give me some suggsetion about emac

  • Guru 67150 points

    In reply to user5954100:

    Hi,

    Thanks for the feedback! Even there is something wrong with the EMAC configuration, I don't expect you spend time to debug it, the TI provided test application is expected to work as it is. If not, we will debug and fix it.

    I got clarification that AM335x NIMU ping was tested on AM335x GP EVM, not the BBB. So, I am looking for BBB to test it and will update you.

    Regards, Eric
  • In reply to lding:

    Thanks for the feedback!I will wait you test result.please let me know the result as you havee tested

  • Guru 67150 points

    In reply to user5954100:

    Hi,

    I found a BBB board and tested, it worked for me. Attached is the binary, please try it if it worked for you. I tested "ping 192.168.1.4" with it.NIMU_BasicExample_bbbAM335x_armExampleproject.out

    Regards, Eric

  • In reply to lding:

    Hi Eric

        Thank you for youre feedback,I have download you bin file to my board,the log show:

    --------------------------------------------------------------------------------------
    RX | Good: 0 | Bcast: 0 | Mcast: 0 | Oct: 0 |
    RX | Pause: 0 | CRC: 0 | AlignErr: 0 | Oversz: 0 |
    RX | Jabber: 0 | Undersz: 0 | Frag: 0 | Filt: 0 |
    RX | QoS: 0 | SOFOvr: 0 | MOFOvr: 0 | DMAOvr: 0 |
    TX | Good: 0 | Bcast: 0 | Mcast: 0 | Oct: 0 |
    TX | Pause: 0 | Deferred: 0 | Coll: 0 | Udrn: 0 |
    --------------------------------------------------------------------------------------
    ENETPHY_FindingState: Timed Out looking for a Phy!
    ENETPHY_FindingState: Timed Out looking for a Phy!
    ENETPHY_FindingState: Timed Out looking for a Phy!
    ENETPHY_FindingState: Timed Out looking for a Phy!
    --------------------------------------------------------------------------------------
    RX | Good: 0 | Bcast: 0 | Mcast: 0 | Oct: 0 |
    RX | Pause: 0 | CRC: 0 | AlignErr: 0 | Oversz: 0 |
    RX | Jabber: 0 | Undersz: 0 | Frag: 0 | Filt: 0 |
    RX | QoS: 0 | SOFOvr: 0 | MOFOvr: 0 | DMAOvr: 0 |
    TX | Good: 0 | Bcast: 0 | Mcast: 0 | Oct: 0 |
    TX | Pause: 0 | Deferred: 0 | Coll: 0 | Udrn: 0 |
    --------------------------------------------------------------------------------------
    ENETPHY_FindingState: Timed Out looking for a Phy!
    ENETPHY_FindingState: Timed Out looking for a Phy!
    ENETPHY_FindingState: Timed Out looking for a Phy!
    ENETPHY_FindingState: Timed Out looking for a Phy!

    and I still can't ping successful

  • In reply to user5954100:

    my board has 1 poart,and the Chip configuration is MMI1,
    I have modified the pinmux_data.c that match my board.shall I modify the EMAC_soc init config?
    myy PDK version is pdk_am335x_1_0_13
  • Guru 67150 points

    In reply to user5954100:

    Hi,

    What board you are using? Is it TI Beagle board black or your own board? Why you need to modify pinmux_data.c? If you modify the PINMUX, then you also need to rebuild the board library. See:
    software-dl.ti.com/.../index_board.html

    The error came from ENET_PHY_log("ENETPHY_FindingState: Timed Out looking for a Phy!\n"); You need check the enet_phy.c for your own board to see why the PHY can't be found.

    Also, if you are using MII instead of RMII, you should use:
    /* Chip configuration MII/RMII selection */
    SOCCtrlCpswPortMacModeSelect(1, ETHERNET_MAC_TYPE_MII);
    SOCCtrlCpswPortMacModeSelect(2, ETHERNET_MAC_TYPE_MII);

    Regards, Eric
  • In reply to lding:

    I am using our own board,and I have checked that the pinmux is the same with Beagle board.
    I have modified :
    /* Chip configuration MII/RMII selection */
    SOCCtrlCpswPortMacModeSelect(1, ETHERNET_MAC_TYPE_MII);
    SOCCtrlCpswPortMacModeSelect(2, ETHERNET_MAC_TYPE_MII);

    but it is still unworked.
  • Guru 67150 points

    In reply to user5954100:

    Thanks! Then you need to check your board why it can't find the PHY? Is this the same PHY used in TI BBB and the same circuit design?

    Regards, Eric

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.