• TI Thinks Resolved

Linux/TMDX654IDKEVM: Error Building SDK

Prodigy 180 points

Replies: 1

Views: 54

Part Number: TMDX654IDKEVM

Tool/software: Linux

Hello,

I used the following command to stat the build for SDK as advised here: http://software-dl.ti.com/processor-sdk-linux/esd/docs/05_03_00_07/linux/Overview_Building_the_SDK.html#processor-sdk-build-reference

However, I am getting the following error:

| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qtoolbox'
| cd qopenglwidget/ && ( test -e Makefile || /home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/git/tests/auto/widgets/widgets/qopenglwidget/qopenglwidget.pro -qtconf /home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/bin/qt.conf ) && make -f Makefile
| make[5]: Entering directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qtoolbutton'
| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qtoolbutton'
| make[5]: Entering directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qopenglwidget'
| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qopenglwidget'
| make[4]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets'
| make[3]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets'
| make[2]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto'
| ERROR: oe_runmake failed
| make[1]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests'
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/temp/log.do_compile.6070)
ERROR: Task (/home/prateek/tisdk/oe-layersetup/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile) failed with exit code '1'

Please advise.

Thanks,

Prateek