My EV3 board can run debian 4.0(etch) now.
then I have intalled xserver as "apt-get install xserver-xorg-video-fbdev"
when video output to LCD, run X is ok.
and i make those change
omap_disp_out.c
#if defined(CONFIG_OMAP3EVM_LCD_VGA) || defined(CONFIG_FB_OMAP_LCD_VGA)
#define H4_LCD_XRES 1280 /* Change these */
#define H4_LCD_YRES 720
//#define H4_LCD_XRES 480
//#define H4_LCD_YRES 640
"echo DVI > /sys/class/display_control/omap_disp_control/ch0_output" set output to dvi
the login prompt displayed.
BUT SYSTEM CRASHED WHEN I RUN X.
There is not any error message print to serial console or display.just system hangup.
any body resolve this problem?