Other Parts Discussed in Thread: DRA746
Tool/software: Linux
Hello,
I downloaded the TDAx Linux and RTOS PROCESSOR_SDK for Vision SDK V_03_01_00_00 and compiled for linux. I would like to add packages to the rootfs and make changes to the .config file.
1. I would like to add packages like openvpn or minicom to the linux filesystem. Where can I add these packages to the rootfs?
2. I tried to manually make changes to the .config file using the command make menuconfig in the directiory <PROCESSOR_SDK>/ti_components/os_tools/linux/kernel/omap/
. When I would run the command to recompile the linux rootfs using the command make linux in the directory <PROCESSOR_SDK>/vision_sdk/build/ the .config file, in <PROCESSOR_SDK>/ti_components/os_tools/linux/kernel/omap/, would be restored to default.
Thank you,
iFer