This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

RTOS/TDA2PXEVM: 2MP SV DEMO UG and HW information for TDA2PxEVM

Part Number: TDA2PXEVM

Tool/software: TI-RTOS

Dear Champs,

My customer want to evaluate 2MP SV DEMO using TDA2Px EVM and I found there is new update for this in VisionSDK3.02, but I could not find any UserGuide and details for this. I only find below in the Release notes and 'ProcessorSDK_Vision_IssSensor_TestMatrix.xls', but could not find any other details.

Could you please let me know where I can find details for 2MP SV DEMO?

And also could you please let me know HW configuration for 2MP SV DEMO? It seemed it was implemented on Fusion board. Is this right?

Is it possible to run it on Vision board also? Is additional deserializer needed?

Thanks and Best Regards,

SI.

  • Hi SI,

    This demo is actually supported on Linux build and uses ISS drivers. It captures RAW images from the OV2775 or IMX390 sensors, uses ISS to convert RAW data into YUV and then it uses SGX to stitch the images. It uses fusion board to capture four camera input over CSI2 interface. There is a TIDA1130 module, which supports OV2775 sensor and D3 module, supporting IMX390 sensor. Let me know if you want more information.

    Rgds,

    Brijesh

  • Hi, Sung-IL,

    The query has been forwarded to the VSDK lead.

    Regards,
    Mariya

     Be sure to read the Forum Guidelines and FAQ.

  • In reply to Brijesh Jadav:

    Hi Brijesh,

    Is it 3D SV DEMO?
    To run this DEMO, should they use Fusion application Daughter Board? Is it possible to use Vision application Daughter Board to run this DEMO?
    If not, is there any plan to release 2MP SV DEMO for Vision applicaiton Daughter Board in future releases?
    Is there any plan to release 2MP 2D SV DEMO running on TI-RTOS?

    When we will release detailed document for this 2MP DEMO? When customer buy TDA2+ EVM, can they set-up 2MP DEMO by themselves using VisionSDKv3.02?

    Thanks and Best Regards,
    SI.
  • In reply to Sung-IL:

    Hi SI,

    yes, it is 3D SV demo.
    No This demo is not supported on Vision board, it is supported only on Fusion board and as of now, AFAIK, there is no plan to support 2MP SRV demo using vision daughter card.
    Vision card outputs only on parallel interface and one of the advantage of J6+ is that it support capture over CSI2 serial interface. We are using CSI interface to get 2MP 4Ch data.

    As such, most of the documentation should be available, Let me check what is missing in documents.
    yes, customer can setup 2mp demo using TDA2x+ EVM, fusion board and TIDA1130/IMX390 sensors. They need to use VSDK 3.02 release.

    Regards,
    Brijesh
  • In reply to Brijesh Jadav:

    Hi Brijesh,

    I checked it again, but I could not find any related document. It seemed the 'VisionSDK_UserGuide_2MP_3D_SurroundView.pdf' is not updated yet. the title of 'VisionSDK_UserGuide_2MP_3D_SurroundView' is a 'Vision SDK TDA2xx 2MP 3D Surround View User Guide', not TDA2Px.


    Thanks and Best Regards,
    SI.
  • In reply to Sung-IL:

    SI
    VisionSDK_UserGuide_2MP_3D_SurroundView.pdf is currently for TDApx based 2MP SRV,
    No section added for TDA2Px 2MP SRV, where ISS is getting used.
    Sorry, we do not have any seperate user guide for TDA2Px 2MP 3D SRV, will add one section the same for next release.

    regards, Shiju
  • In reply to Shiju Sivasankaran:

    Hi Shiju,

    Could you please release instruction how customer can try it?
    my customer is willing to buy TDA2P EVM to run this 2D SV DEMO. Is it OK to buy Fusion Kit and TIDA-01130 OV2775 camera module only? or other kit will be required?
    Could you please explain about HW setup at least?

    Thanks and Best Regards,
    SI.
  • In reply to Sung-IL:

    SI

    You need below HW to set-up 2MP SRV demo on TDA2Px

    1. TDA2Px EVM - 1

    2. Fusion Card/EVM - 1

    3. TIDA OV2775 cameras - 4 (with Fakra cables)

    separate power supply is required for Fusion Card

    Regards, Shiju

  • In reply to Shiju Sivasankaran:

    SI
    please make sure you order TIDA OV2775 cameras with Fisheye lens.
    Sometimes, spectrum digital ship only sensor without lens module

    regards, Shiju

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.