Other Parts Discussed in Thread: DRA742, PCF8575, PMP, DRA752, TPD12S015, TLV320AIC3106, DS90UH925Q, WL1835
Tool/software: Linux
Dear TI forum,
we have some issue regarding the development of ethernet daisy chain. We are trying to connect 2 TDA2xx SoCs that are located on our custom-made board, using linux. Eth0 of SoC1 runs directly to the phy and this is working fine. We can ping our PC and send data packets.
However, the RGMII connection between our 2 SoCs is direct, meaning, there is no PHY between them. This connection goes from eth1 of SoC1 to the eth0 of SoC2.
As we have seen, this is something that should be done using fixed-link connection. Is this right? How can we fix this issue and make this daisy chain?
Our device tree for these SoCs looks like this (we are using different builds on 2 SD cards for them):
SoC1 dts:
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <7>;
phy-mode = "rgmii-id";
dual_emac_res_vlan = <1>;
};
&cpsw_emac1 {
fixed-link = <0 1 1000 0 0>;
phy-mode = "rgmii-id";
};
/////////////////////////////////////////////////////////////////////////////////
SoC2 dts:
&cpsw_emac0 {
fixed-link = <0 1 1000 0 0>;
phy-mode = "rgmii-id";
};
/*For testing only, this SoC has no phy*/
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <7>;/*2*/
phy-mode = "rgmii-id";/*rgmii*/
dual_emac_res_vlan = <1>;
};
/////////////////////////////////////////////////////////////////////////////////
SoC1 log:
=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2018.04.18 14:36:46 =~=~=~=~=~=~=~=~=~=~=~=
U-Boot SPL 2016.05 (Apr 11 2018 - 18:26:37)
DRA752-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
Card did not respond to voltage select!
*** Warning - MMC init failed, using default environment
Trying to boot from MMC1
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
Card did not respond to voltage select!
*** Warning - MMC init failed, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05 (Apr 11 2018 - 18:26:37 +0200)
CPU : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x EVM REV
DRAM: 1.5 GiB
MMC: i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
OMAP SD/MMC: 0, OMAP SD/MMC: 1
Card did not respond to voltage select!
*** Warning - MMC init failed, using default environment
Warning: fastboot.board_rev: unknown board revision
Card did not respond to voltage select!
ERROR: invalid mmc device
at arch/arm/cpu/armv7/omap-common/utils.c:189/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: Could not get PHY for ethernet@48484000: addr 2
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 2 1 0
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
switch to partitions #0, OK
mmc0 is current device
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
163 bytes read in 2 ms (79.1 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
switch to partitions #0, OK
mmc0 is current device
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
SD/MMC found on device 0
3552360 bytes read in 178 ms (19 MiB/s)
106863 bytes read in 24 ms (4.2 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x363468 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe2000, end 8ffff16e ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.84 (root@rtrkn096-lin) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #12 SMP PREEMPT Fri Apr 13 17:46:06 CEST 2018
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA742
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[ 0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000bfd00000 to fe600000 for dram barrier
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @ef62b000 s14912 r8192 d21952 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 243264
[ 0.000000] Kernel command line: console=ttyS0,115200n8 vram=16M root=PARTUUID=5d173897-02 rw rootwait ip=none mem=1024M
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 410840K/979968K available (6619K kernel code, 319K rwdata, 2388K rodata, 340K init, 290K bss, 364328K reserved, 204800K cma-reserved, 234496K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08d402c (9009 kB)
[ 0.000000] .init : 0xc08d5000 - 0xc092a000 ( 340 kB)
[ 0.000000] .data : 0xc092a000 - 0xc0979d60 ( 320 kB)
[ 0.000000] .bss : 0xc097b000 - 0xc09c3800 ( 290 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000015] Switching to timer-based delay loop, resolution 162ns
[ 0.000326] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000334] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000763] Console: colour dummy device 80x30
[ 0.000784] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000797] pid_max: default: 32768 minimum: 301
[ 0.000894] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000904] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001441] Initializing cgroup subsys io
[ 0.001457] Initializing cgroup subsys memory
[ 0.001482] Initializing cgroup subsys devices
[ 0.001494] Initializing cgroup subsys freezer
[ 0.001505] Initializing cgroup subsys perf_event
[ 0.001516] Initializing cgroup subsys pids
[ 0.001543] CPU: Testing write buffer coherency: ok
[ 0.001742] /cpus/cpu@0 missing clock-frequency property
[ 0.001758] /cpus/cpu@1 missing clock-frequency property
[ 0.001769] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001801] Setting up static identity map for 0x80008380 - 0x800083e0
[ 0.080066] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080135] Brought up 2 CPUs
[ 0.080147] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080154] CPU: All CPU(s) started in HYP mode.
[ 0.080160] CPU: Virtualization extensions available.
[ 0.080536] devtmpfs: initialized
[ 0.109027] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.110005] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.313610] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.313630] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.317859] pinctrl core: initialized pinctrl subsystem
[ 0.318714] NET: Registered protocol family 16
[ 0.319642] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.350237] cpuidle: using governor ladder
[ 0.380265] cpuidle: using governor menu
[ 0.388700] OMAP GPIO hardware version 0.1
[ 0.392643] omap_gpio 4805d000.gpio: could not find pctldev for node /ocp/l4@4a000000/scm@2000/pinmux@1400/gpio6_pins, deferring probe
[ 0.392658]
[ 0.392658]
[ 0.394580] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.410591] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 0.410604] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.419811] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.419822] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.420280] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.420289] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.420885] OMAP DMA hardware revision 0.0
[ 0.461515] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.462669] edma 43300000.edma: memcpy is disabled
[ 0.467278] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.467937]
[ 0.467937]
[ 0.471668] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.471846] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.472005] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.472170] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.472459] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.472645] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.475648] palmas 0-0058: IRQ missing: skipping irq request
[ 0.491093] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
[ 0.552900]
[ 0.552900]
[ 0.553232] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.553633] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.553837] media: Linux media interface: v0.10
[ 0.553889] Linux video capture interface: v2.00
[ 0.553928] pps_core: LinuxPPS API ver. 1 registered
[ 0.553936] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.553959] PTP clock support registered
[ 0.554009] EDAC MC: Ver: 3.0.0
[ 0.554750] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.555048] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.555377] Advanced Linux Sound Architecture Driver Initialized.
[ 0.556217] clocksource: Switched to clocksource arch_sys_counter
[ 0.566697] NET: Registered protocol family 2
[ 0.567196] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.567259] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.567384] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.567430] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.567460] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.567670] NET: Registered protocol family 1
[ 0.567930] RPC: Registered named UNIX socket transport module.
[ 0.567939] RPC: Registered udp transport module.
[ 0.567945] RPC: Registered tcp transport module.
[ 0.567951] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.568946] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.578907] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.579559] NFS: Registering the id_resolver key type
[ 0.579584] Key type id_resolver registered
[ 0.579592] Key type id_legacy registered
[ 0.579653] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.580912] bounce: pool size: 64 pages
[ 0.581063] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.581077] io scheduler noop registered
[ 0.581089] io scheduler deadline registered
[ 0.581125] io scheduler cfq registered (default)
[ 0.586008] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.589236] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[ 0.589248] No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[ 0.589281] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.589303] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.619455] dra7-pcie 51000000.pcie_rc: link is not up
[ 0.619631] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[ 0.619644] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.619655] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.619665] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.620075] PCI: bus0: Fast back to back transfers disabled
[ 0.620197] PCI: bus1: Fast back to back transfers enabled
[ 0.620282] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.620297] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.620309] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.620528] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.680332] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.683708] console [ttyS0] disabled
[ 0.683762] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 269, base_baud = 3000000) is a 8250
[ 1.729833] console [ttyS0] enabled
[ 1.734226] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 270, base_baud = 3000000) is a 8250
[ 1.743922] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 271, base_baud = 3000000) is a 8250
[ 1.753960] [drm] Initialized drm 1.1.0 20060810
[ 1.760001] OMAP DSS rev 6.1
[ 1.763745] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 1.779520] loop: module loaded
[ 1.783040] vmemexp device MAJOR num = 246
[ 1.787193] vmemexp class registered
[ 1.790905] /dev/vmemexp device registered
[ 1.795020] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[ 1.800705] nand: No NAND device found
[ 1.804476] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[ 1.811503]
[ 1.823577] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
[ 1.829173] 7 ofpart partitions found on MTD device spi32766.0
[ 1.835032] Creating 7 MTD partitions on "spi32766.0":
[ 1.840209] 0x000000000000-0x000000040000 : "QSPI.SPL"
[ 1.846354] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 1.852677] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[ 1.859622] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 1.866317] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 1.873699] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[ 1.880068] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[ 1.887856] libphy: Fixed MDIO Bus: probed
[ 1.894057]
[ 1.904192] cpsw 48484000.ethernet: Missing dual_emac_res_vlan in DT.
[ 1.910886] cpsw 48484000.ethernet: Using 2 as Reserved VLAN for 1 slave
[ 1.917657] cpsw 48484000.ethernet: Detected MACID = c8:fd:19:ba:83:8a
[ 1.924310] cpsw 48484000.ethernet: cpts: overflow check period 800
[ 1.931309] cpsw 48484000.ethernet: cpsw: Detected MACID = c8:fd:19:ba:83:8b
[ 1.939957] mousedev: PS/2 mouse device common for all mice
[ 1.946126] i2c /dev entries driver
[ 1.954924]
[ 1.964648] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 1.971257] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 1.977833] evm_3v3_sw: supplied by sysen1
[ 2.146712]
[ 2.156279] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.164877] aic_dvdd: supplied by evm_3v3_sw
[ 2.169835]
[ 2.180007] davinci-mcasp 4847c000.mcasp: invalid tdm slots: 0
[ 2.187665] NET: Registered protocol family 10
[ 2.202985] sit: IPv6 over IPv4 tunneling driver
[ 2.208224] NET: Registered protocol family 17
[ 2.212898] Key type dns_resolver registered
[ 2.217312] omap_voltage_late_init: Voltage driver support not added
[ 2.224195] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.230418] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.237118] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.243325] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.251548] Power Management for TI OMAP4+ devices.
[ 2.256643] Registering SWP/SWPB emulation handler
[ 2.263519] dmm 4e000000.dmm: initialized all PAT entries
[ 2.270861] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.277541] [drm] No driver support for vblank timestamp query.
[ 2.283843] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.300563]
[ 2.316498] pcf857x: probe of 0-0020 failed with error -121
[ 2.322269]
[ 2.331632] pcf857x: probe of 0-0021 failed with error -121
[ 2.337413]
[ 2.396233] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 2.402530] davinci_mdio 48485000.mdio: detected phy mask ffffff7f
[ 2.420572] libphy: 48485000.mdio: probed
[ 2.424599] davinci_mdio 48485000.mdio: phy[7]: device 48485000.mdio:07, driver Marvell 88E1111
[ 2.433795] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.476518]
[ 2.486905] asoc-simple-card sound0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[ 2.495968]
[ 2.514164] [ 2.526191] hctosys: unable to open rtc device (rtc0)
[ 2.539318] evm_1v8: disabling
[ 2.542390] aic_dvdd: disabling
[ 2.545715] ldousb: disabling
[ 2.549105] ALSA device list:
[ 2.552082] #0: DRA7xx-EVM
[ 2.555612] Waiting for root device PARTUUID=5d173897-02...
[ 3.103304] mmc2: host does not support reading read-only switch, assuming write-enable
[ 3.113263] mmc2: new high speed SDHC card at address 59b4
[ 3.129127] mmcblk0: mmc2:59b4 USD 7.36 GiB
[ 3.134357] mmcblk0: p1 p2
[ 3.137706]
[ 3.216974] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
[ 3.225676] EXT4-fs (mmcblk0p2): couldn't mount as ext2 due to feature incompatibilities
[ 3.626462] EXT4-fs (mmcblk0p2): recovery complete
[ 3.639842] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.648010] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 3.660148] devtmpfs: mounted
[ 3.663317] Freeing unused kernel memory: 340K
[ 3.667794] This architecture does not have kernel memory protection.
[ 3.895808] systemd[1]: System time before build time, advancing clock.
[ 3.952655] random: systemd: uninitialized urandom read (16 bytes read, 15 bits of entropy available)
[ 3.965663] random: systemd: uninitialized urandom read (16 bytes read, 15 bits of entropy available)
[ 3.977447] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 3.995939] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.12!
[ 4.017078] systemd[1]: Set hostname to <dra7xx-evm>.
[ 4.078966] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
[ 4.089082] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
[ 4.099779] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
[ 4.137761] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 18 bits of entropy available)
[ 4.150169] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 18 bits of entropy available)
[ 4.244471] random: systemd: uninitialized urandom read (16 bytes read, 21 bits of entropy available)
[ 4.254007] random: systemd: uninitialized urandom read (16 bytes read, 21 bits of entropy available)
[ 4.263980] random: systemd: uninitialized urandom read (16 bytes read, 21 bits of entropy available)
[ 4.608984] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[ 4.616864] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[ 4.624561] systemd[1]: sysinit.target: Found dependency on basic.target/start
[ 4.631855] systemd[1]: sysinit.target: Found dependency on sockets.target/start
[ 4.639339] systemd[1]: sysinit.target: Found dependency on dbus.socket/start
[ 4.646524] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[ 4.653955] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[ 4.663407] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[ 4.698804] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.717716] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 4.736543] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.757012] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 4.776408] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 4.796971] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 4.826517] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 4.846496] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.896634] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 4.929279] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 4.948714] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...[ 4.960778] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 4.991092] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 5.018509] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 5.046645] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 5.076512] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 5.096606] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 5.116527] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 5.146996] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 5.206399] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 5.226424] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 5.260772] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 5.286687] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 5.316488] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 5.336465] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 5.396446] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 5.432719] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 5.456502] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 5.476467] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 5.496607] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[ OK ] Started Remount Root and Kernel File Systems.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Started Setup Virtual Console.
Starting Apply Kernel Variables...
Starting udev Coldplug all Devices...
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 6.220513] systemd-journald[144]: Received request to flush runtime journal from PID 1
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Mounting /media/ram...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started udev Coldplug all Devices.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
[ 6.715480] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 6.729457] remoteproc0: 55020000.ipu is available
[ 6.734382] remoteproc0: Note: remoteproc is still under development and considered experimental.
Starting Create Volatile Files and Directories...[ 6.751898] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ OK ] Started Load/Save Random Seed.[ 6.780680] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
[ 6.806326] remoteproc1: 40800000.dsp is available
[ OK ] Started Create Volatile Files and Directories.[ 6.856937] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 6.905656] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[[;32m OK ]Found device /dev/ttyS0.[ 6.923465]
[ 6.923609] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
[ 6.923651] remoteproc2: 41000000.dsp is available
[ 6.923654] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 6.923656] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 7.017680] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
tSarting Update UTMP about System Boot/Shutdown...[ 7.050479]
taSrting Network Time Synchronization...
[ 7.140519] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 7.195806]
[[;32m OK ]Started Update UTMP about System Boot/Shutdow.
[ 7.718502] remoteproc1: registered virtio0 (type 7)
[ 7.884492] remoteproc0: registered virtio1 (type 7)
[ 7.904694]
[ 7.942371] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 7.950816]
[ 7.996337] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc0
[ 8.003997] CAN device driver interface
[ 8.009265]
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
Starting Synchronize System and HW clocks...
[ 8.144428] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=326)
[ 8.166598]
[ 8.230816] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 8.237620] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 8.243702]
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Reached target System Initialization.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ 8.430885] SCSI subsystem initialized
[ OK ] Reached target Timers.
[ 8.597480] remoteproc2: registered virtio2 (type 7)
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ 8.720844]
[ OK ] Reached target Basic System.
[ 8.735806]
[ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
Starting uim-sysfs.service...
Starting Print notice about GPLv3 packages...
Starting Login Service...
Starting Telephony service...
[ OK ] Started Kernel Logging Service.
Starting TI MultiCore Tools Daemon...
Starting Permit User Sessions...
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started System Logging Service.
[ OK ] Started D-Bus System Message Bus.
[ 9.156867] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
[ 9.171015]
[ 9.256611] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 9.264920]
[ 9.274797] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 9.296679]
[ 9.305959] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 9.347447] scsi host0: ahci
[ 9.350676] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 310
[ 9.370736]
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Telephony service.
[ 9.716280] ata1: SATA link down (SStatus 0 SControl 300)
Starting Network Service...
Starting Save/Restore Sound Card State...
[FAILED] Failed to start TI MultiCore Tools Daemon.
See 'systemctl status ti-mct-daemon.service' for details.
[ OK ] Started Permit User Sessions.
[ OK ] Started Save/Restore Sound Card State.
[ 10.095824] Bluetooth: Core ver 2.21
[ 10.114822] net eth1: initializing cpsw version 1.15 (0)
[ 10.122973] NET: Registered protocol family 31
[ 10.130025] NET: Registered protocol family 15
[ OK ] Started Network Service.
[ 10.149342] Bluetooth: HCI device and connection manager initialized
[ 10.150406] net eth0: initialized cpsw ale version 1.4
[ 10.150410] net eth0: ALE Table size 1024
[ 10.153317] net eth1: phy found : id is : 0x0
[ 10.192439]
[ 10.192439]
[ 10.192439] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 10.222743] Bluetooth: HCI socket layer initialized
[ 10.222752] Bluetooth: L2CAP socket layer initialized
[ 10.222780] Bluetooth: SCO socket layer initialized
[ 10.461206] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 10.588227] Initializing XFRM netlink socket
[ 10.619032] remoteproc1: powering up 40800000.dsp
[ 10.650212] remoteproc1: Booting fw image dra7-dsp1-fw.xe66, size 7449540
[ 10.672449] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
[ 10.678344] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[ 10.684321] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[ 10.710397] net eth0: initializing cpsw version 1.15 (0)
[ 10.812547] remoteproc1: remote processor 40800000.dsp is now up
[ 10.823564] net eth0: phy found : id is : 0x1410cc2
[ 10.834417] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 10.846563]
[ 10.866609] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 10.899197] remoteproc0: powering up 55020000.ipu
[ 10.908675]
[ 10.978549] remoteproc0: Booting fw image dra7-ipu2-fw.xem4, size 9507944
[ 10.999907]
[ 11.012074] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ OK ] Started uim-sysfs.service.
[ 11.039462]
[ 11.050631] random: nonblocking pool is initialized
[ 11.072338]
[ 11.123154] remoteproc0: remote processor 55020000.ipu is now up
[ 11.140997] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 11.157508]
[ 11.167629] remoteproc2: powering up 41000000.dsp
[ 11.173023]
[ 11.190967] remoteproc2: Booting fw image dra7-dsp2-fw.xe66, size 7449540
[ 11.201178]
[ 11.212922] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
[ 11.218988] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
[ 11.224910] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
[ 11.295746] remoteproc2: remote processor 41000000.dsp is now up
[ 11.381496] virtio_rpmsg_bus virtio1: creating channel rpmsg-proto addr 0x50
[ 11.391130] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x50
[ 11.411799] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 11.417777]
[ 11.429088] virtio_rpmsg_bus virtio2: creating channel rpmsg-proto addr 0x50
[ 11.444317]
[ 11.463343] NET: Registered protocol family 41
[ 11.482835]
Starting rc.pvr.service...
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Reached target Network.
Starting Network Name Resolution...
Starting Lightning Fast Webserver With Light System Requirements...
[ OK ] Reached target Sound Card.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Started Getty on tty1.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Network Name Resolution.
[ OK ] Started Login Service.
[ 11.768290] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ OK ] Started rc.pvr.service.
Starting weston.service...
[ OK ] Started weston.service.
Starting tiipclad-daemon.service...
Starting telnetd.service...
[ OK ] Started telnetd.service.
[ OK ] Started tiipclad-daemon.service.
Starting thttpd.service...
[ OK ] Started thttpd.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.[ 12.146282] cpsw 48484000.ethernet eth1: Link is Up - 1Gbps/Full - flow control off
[ 12.156138] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
Starting gdbserverproxy.service...
[ OK ] Started gdbserverproxy.service.
Starting matrix-gui-2.0.service...
[ OK ] Started matrix-gui-2.0.service.
Starting thermal-zone-init.service...
[ OK ] Started thermal-zone-init.service.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
binutils-dev
binutils
bison-dev
bison
cpp-symlinks
cpp
dosfstools
g++-symlinks
g++
gawk-dev
gawk
gcc-symlinks
gcc
gdb
gdbc6x
gdbserver
gstreamer1.0-libav
libcairo-perf-utils
libgmp10
libidn11
libmpc3
libmpfr4
m4-dev
m4
make
nettle
parted
swig-dev
swig
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dra7xx-evm ttyS0
Arago 2016.12 dra7xx-evm ttyS0
dra7xx-evm login: