Tool/software: Code Composer Studio
hi,
I am using C6657 and mcsdk for multcore develop, and faced a problem that debug mode cannot into main function.
So i run demo which from sdk, i am only modify cfg file in order to use more than 256M ddr. and the same problem happened.
Can you help?
modify \ti\mcsdk_2_01_02_06\demos\hua\evmc6657l\evm.cfg
/*
** Heap Management Module - Create a default Heap.
*/
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var heapMemParams = new HeapMem.Params();
heapMemParams.size = 235*1024*1024; //0xF4240; /* 1Mb*/ <-------------- modify here to use more than 256M ddr, and demo cannot running into main function
heapMemParams.sectionName = "systemHeap";
Program.global.heap0 = HeapMem.create(heapMemParams);
Memory.defaultHeapInstance = Program.global.heap0;
/* Load the CSL package - LoadPackage is equivalent to linking the library */
var Csl = xdc.loadPackage('ti.csl');