Tool/software: TI-RTOS
Hi TI Experts,
Please let me confirm the following question.
[Question]
Does TI provide the NDK supported function list as RFC?
Best regards.
Kaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi hajime,
A1: These RFCs are supported:
RFC 768 : UDP
RFC 783 : TFTP
RFC 791 : IP
RFC 792 : ICMP
RFC 793 : TCP
RFC 826 : ARP
RFC 854 : Telnet
RFC 1034, 1035 : DNS
RFC 2131 : DHCP
RFC 2460 : IPv6
RFC 2616 : HTTP/1.1
Above block diagram may give a overview of what's supported in NDK.
[Q2] The road map of NDK feature depends on customer needs. If you have specific RFC request, we can evaluate to include.
Regards,
Garrett