I'm using the usb in my project to transmit data and have encountered a problem with the CPPI DMA,
when i try to put a packet into one of the submission queues for the TX endpoints, it instead ends up in queue 60.
i dont know how this happens, i dont know why it happens either, and it prevents me from being able to use the CPPI DMA properly.
and to clarify, im using the CPPI DMA for RX as well and that works fine, its only tx thats giving me troubles.
ive tried running the USB DMA example from the csl and the same thing keeps happening.
help?
EDIT: my IDE is Code Composer 6, and the csl version is 3.08.00.01
the output from the USB DMA EXAMPLE is:
reset done
usb init done
usb open done
config done
reset dev done
request ep 0 done
config ep 0 done
request ep 1 done
config ep 1 done
ep setup done
set params done
connect dev done