Hi,
I'm trying to format the included SD card for the TDA2P board in order to boot from it.
When I try to format from the command line, I get a "The specified cluster size is too small for FAT32" error. When I try to format using diskpart, I get "The cluster size is too small" error.
When I load the generated Appimage and MLO onto the unformatted SD card, the TDA2P is unable to boot from it.
I have also tried to format a store-bought SD card, but get the same cluster size errors.
How can I correctly format the SD card to boot from it?
Thanks,
Richard