This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

RTOS/AM5728: PCIe - How to Retrieve EP BAR

Prodigy 180 points

Replies: 16

Views: 575

Part Number: AM5728

Tool/software: TI-RTOS

I'm running TIRTOS on AM5728 SOM with a Microsemi Igloo2 FPGA PCIe device plugged into the PCIe slot.  I have a successful linked up and can access the EP vendor and device info.   However, I'm having difficulty with figuring how to access the EP BAR addresses so i can turn on/off the its LEDs.  Base on the Linux device driver for this device, i need to use the BAR0 + LED_OFFSET.  Can I use the same method?  It is so, how can i request the BAR addresses from the FPGA?

Thanks.

  • Hello!

    During enumeration process root complex assigns base addresses to BARs of endpoint, so RC knows those base addresses. However, there is no way for RC to know actual layout of memory or i/o device behind that BAR. In other words, RC should have prior knowledge about layout of EP. After that theses are simple accesses like BARx + OFFSET.

  • In reply to rrlagic:

    Thanks for helping.  I'm new to this; so I've more questions that i hope you could help:  With the layout of i/o device, is using the outbound address as base address and access the i/o possible (I've only one i/o)?  or do  i need to call Pcie_cfgBar() to configure the i/o BARs? if calling Pcie_cfgBar() is the only option, do i use the size of each memory windows to set the barCfg.base with the first one set to zero?  or can i pick an available address location within my RC memory map for those i/o BARs?

  • In reply to Jodat Vu:

    My I/O vendor provides these information: for BAR0, 0x4_0000 as local to translate to 0x4000_0000. I used 0x4000_0000 in the following code block:

    barCfg.location = pcie_LOCATION_REMOTE;
    barCfg.mode = pcie_EP_MODE;
    barCfg.base = FPGA_BAR0_BASE;
    barCfg.prefetch = pcie_BAR_NON_PREF;
    barCfg.type = pcie_BAR_TYPE32;
    barCfg.memSpace = pcie_BAR_MEM_MEM;
    barCfg.idx = 0;

    if ((retVal = Pcie_cfgBar(handle, &barCfg)) != pcie_RET_OK)
    {
    PCIE_logPrintf ("Failed to configure FPGA BAR0 (%d)\n", (int)retVal);
    exit(1);
    }

    Later on, I requested the type0BarIdx, the results are: raw = 0x4000_0000; but base = 0x0400_0000

    Which one should I use as BAR0 for the i/o? Using the memory browser, it shows the 0x4000_0000 with "-------" to indicate no-read region.

    I'm using the pcie_sample.c as the test driver.
  • Guru 56610 points

    In reply to Jodat Vu:

    Hi,

    In your case, the AM572x is the PCIE RC running TI-RTOS code. The FPGA is the PCIE EP. You have the linked up successfully.

    The data access (R/W) from AM572x side looks like below (I use PCIESS1 here for simplicity):

    • The CPU access (R/W) the the PCIe_SS1 Configuration space address 0x2xxx_xxxx
    • There is outbound translation setup to convert this 0x2xxx_xxxx to PCIE address. The pcie_sample.c code has two outbound regions:
    1. OB region 0 used to access remote EP configuration space offset 0x1000 to 0x1FFC. So if you look at 0x2000_1000 you should be able to access FPGA side configuration space, starting from device id/vendor id. E.g., 0x2000_1010 you should be able to access BAR0 of FPGA.
    2. OB region 1 used to access remote EP memory space offset 0x0100_0000 with 16MB window. So, if you want to access FPGA side data space, you need to look at 0x2100_0000 and onwards. This OB setup the outbound access to 0x7000_0000. It means when you look at 0x2100_0000 on RC side, the PCIE address cross the connection is 0x7000_0000. Then in your FPGA side, you need an inbound mapping of this 0x7000_0000 into some internal memory.

    Given you know that there is a fixed mapping for FPGA side: 0x4_0000 as local to translate to 0x4000_0000.

    What you need to do:

    1. In the RC side for the OB1, you need to change 0x7000_0000 to 0x4_0000
    2. In the RC side you need to do a Pcie_cfgBar() for the remote BAR with barCfg.base = 0x4_0000; From RC side 0x2000_1010 you can cross-check this value.

    What happened is: on RC side, you W/R 0x2100_0000, it translates to 0x4_0000 over the PCIE interface. Then this address is accepted at the FPGA side with BAR matched. Then the FPGA converts the 0x4_0000 into 0x4000_0000. If you know the LED offset, you should be able to access it with 0x2100_0000 + offset (subject to earlier configured 16MB window size).  

    Regards, Eric

  • In reply to lding:

    hi Eric,

    Thanks for the tutorial.  I've a better understanding, but I still can't command the EP to turn the its LEDs on/off.  Maybe, I didn't do step #2 correctly.

    I can't cross check the value on step #2.  A memory view at 0x2000_1010 shows 0x0000_0000.  Should I see 0x40000 at 0x2100_1010?

    For step #1, I changed the PCIE_OB_LO_ADDR_RC from 0x70000000 to 0x40000

    For step #2, i added the following Pcie_cfgBar() right after the pcieWaitLinkUp() an pcieCheckLinkParams(handle).  The call was successful.

      barCfg.location = pcie_LOCATION_REMOTE;
      barCfg.mode     = pcie_EP_MODE;
      barCfg.base     = 0x40000;
      barCfg.prefetch = pcie_BAR_NON_PREF;
      barCfg.type     = pcie_BAR_TYPE32;
      barCfg.memSpace = pcie_BAR_MEM_MEM;
      barCfg.idx      = 0;

      if ((retVal = Pcie_cfgBar(handle, &barCfg)) != pcie_RET_OK)
      {
        PCIE_logPrintf ("Failed to configure FPGA BAR0 (%d)\n", (int)retVal);
        exit(1);
      }

  • Guru 56610 points

    In reply to Jodat Vu:

    Hi,

    Yes, you should see that BAR0 of your FPGA is 0x0004_0000. How many BARs you have on FPGA side? If you have only one BAR (that is BAR0). The code in step 2 looks right but seems the FPGA didn't take it. Is your BAR0 a memory BAR or I/O BAR? WIll below help?

    barCfg.location = pcie_LOCATION_REMOTE;
    barCfg.mode = pcie_EP_MODE;
    barCfg.base = 0x40000;
    barCfg.prefetch = pcie_BAR_NON_PREF;
    barCfg.type = pcie_BAR_TYPE32;
    barCfg.memSpace = pcie_BAR_MEM_IO;
    barCfg.idx = 0;

    if ((retVal = Pcie_cfgBar(handle, &barCfg)) != pcie_RET_OK)
    {
    PCIE_logPrintf ("Failed to configure FPGA BAR0 (%d)\n", (int)retVal);
    exit(1);
    }

    Can you let me know how the 0x2101_1000 to 0x2101_1024 looks like from AM57x side? This should be your FPGA's VENDOR_DEVICE_ID, STATUS_COMMAND, .... BAR0, ... BAR5. If you manually change the 0x2101_1010 through CCS memory window to values like 0x0004_0000 or 0x0004_0001, or 0x0004_0008 or 0x0004_0009 (save the time for debug purpose, w/o change code and reload and run). Will it help?

    Do you have a way to program the BAR register on FPGA side directly (instead of programming it from AM57x remotely)?

    Regards, Eric
  • In reply to lding:

    The EP has 2 BARs (BAR0 maps to 0x4_0000 and BAR1 maps to 0x2_0000) and we have no way to program to EP BAR registers directly.

    0x21xx_xxxx shows all 0xFFFFFFFF

    However, 0x2000_1000 shows:

    0x20001000  11AA11AA 00100000 00000000 00000000 00000000

    0x20001014  00000000  00000000  00000000  00000000 00000000

    0x20001028  00000000  000011AA 00000000 00000000 00000000

    0x2000103C  00000100 00000000 02126160 00000000 00000000

    0x20001050   00817805 02000000 00000000 00000000 00000000

    0x20001064   00000000 00007811 00000000 00000000 00000000

    0x20001078   48038001 00000008 02020010 10008FE1 000B2810

    0x2000108C   01068C41 10110000 00000000 00000000 00000000

    0x200010A0   00000000 00000000 00000000 00000000 00000000

  • In reply to Jodat Vu:

    hi Eric,
    I found these settings in the .cfg file; what are they for? do i need to change them for my EP? Thanks.
    var peripheralBaseAddrs = [
    { base: 0x4ae00000, size: 0x00100000 }, // PRM
    { base: 0x51000000, size: 0x00800000 }, // pcie_ss1 regs
    { base: 0x51800000, size: 0x01000000 }, // pcie_ss2 regs
    { base: 0x20000000, size: 0x10000000 }, // pcie_ss1 data
    { base: 0x30000000, size: 0x10000000 }, // pcie_ss2 data
  • Guru 56610 points

    In reply to Jodat Vu:

    Hi,

    { base: 0x51000000, size: 0x00800000 }, // pcie_ss1 regs
    { base: 0x51800000, size: 0x01000000 }, // pcie_ss2 regs
    { base: 0x20000000, size: 0x10000000 }, // pcie_ss1 data
    { base: 0x30000000, size: 0x10000000 }, // pcie_ss2 data

    They are PCIE register memory space and data memory space, the SYSBIOS uses those information (starting address and length) to setup MMU, you don't need to change that.

    Regards, Eric
  • Guru 56610 points

    In reply to lding:

    Hi,

    So the FPGA side you have two BARs, you mentioned that LED is accessed by BAR0+OFFSET, is this correct? Or it is BAR1+OFFSET? What is the OFFSET value? Typically BAR0 is automatically pointed (hard wired) to the the PCIE configuration space in the PCIE EP side, this is the design of TI PCIE module. I am not sure if the same on the FPGA side.

    From your access of 0x2000_1000, as I saw offset 0x0 value 0x11AA11AA=====> is this your vendor/device id? offset 0x80 showed 02020010 ====> so you got GEN2 speed with 2 lanes, correct?

    I want to try 1) if you can find out the BAR0 mask value (what you setup for the BAR0 mask?) and 2) change the BAR0 address, from the RC side by poking the 0x2000_1010 address.

    For 1) One way to verify if the BAR Mask registers have been set correctly is to write the pattern values into BAR registers and see if the bits have been masked correctly. For example, you have pre-set BAR0 MASK = 0x0000_3FFF. You write BAR0 = 0xFFFF_FFFF; BAR0 should be read as 0xFFFF_C000 because the lower bits of BAR0 have been masked.

    For 2) Try to change BAR0 to 0x0004_0000 or 0x0004_0001, or 0x0004_0008 or 0x0004_0009. Will you see the value reflected in CCS? Or you still see BAR0 = 0?

    Regards, Eric

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.