Hey,
I am setting up the ar0220 sensor with UB953 to TDA2px. When I set the backchannel frequency to 50mbps as recommended for UB953 the serdes link does not work because the serializer can´t be reached via i2c. I already searched the forum and apparently more people have the same problem, but since their threads weren´t solved, I decided to ask again.
With backchannel frequency set to 25mbps the connection is working fine.
Also I tried the setup with the exact same initialisation for serdes on the TDA3rvp and there it works right away without any problems.
How come that 50mbps works fine with tda3rvp (also UB960) but on tda2px it results in an unreachable serializer?
In another thread someone said he just had to retry writing to the serializer several times and then it would work at one point, I tried that but it didn´t work for me.
I am using PSDK3.3.
best regards,
Nicolas Rausch